Captured to 最爱ADI放大器之AD623 wiki page

最爱ADI放大器之AD623

       去年曾做过一个光电传感器相关的设计,其中模电部分需要将光电二极管的小信号与调零电位器电压相减后再放大50到100倍交由ADC转换,出于成本和需求考虑,ADC直接使用ATMEGA系列单片机自带的10bit ADC,初版设计的时候采用的是LM358运放组成减法器,后来发现由于电阻温飘与放大器偏移等问题导致在不同环境下输出偏移较大,不利于数字系统分析判断状态。而用LM324等运放搭建仪表放大电路也存在电阻匹配以及温飘问题。后来在图书馆查询资料时候看到了一本ADI的运放手册,上面介绍到了AD623,于是迅速去买了几片并画板测试。

       AD623是为单电源优化的集成式仪表放大器,它的增益漂移以及输入电压漂移非常低,能为传感器提供良好的长期稳定性和温度稳定性,其0.35%的高增益精度和低至3μV p-p、35 nV/√Hz的噪音更是可以轻松搭配高位ADC实现高精度测量,很高的CMRR,同时还具有轨对轨特性。虽然AD623是为单电源优化的,其在双电源供电下依然能提供相差无几的性能。需要注意的是,AD623采用的是3运放的标准仪表放大器电路,故如果在单电源状态下工作,输入信号的共模电压需要贴近VCC/2才能获得最高的最大放大倍数,所以在设计阶段计算最高放大倍数时一定要注意共模输入范围。

       总结起来AD623是一款简单易用的仪表放大器,具有良好的性能和相对低廉的价格,在首次使用AD623之后,每每遇到小信号放大场合,诸如电偶测温、电流测量等设计,我都会使用AD623来实现设计。

       以下放出前面提到的光电传感器项目电路图和文件,由于成本和体积限制,本设计采用的是电荷泵产生负轨使AD623工作在双电源下,最终运行效果完全达到设计要求。板载的除了AD623组成的放大电路、LDO、电荷泵、MCU以外还有一个驱动光源的恒流源。