Post Go back to editing

最爱ADI放大器---AD823

最爱ADI放大器---AD823

我是用在光伏并网逆变器上的,用于对光伏的输入电流,交流的输出电压、电流、进行采样和放大。

1AD823的轨到轨输出:结合DSP芯片,两者都采用3.3V供电时,AD823的最高输出正好是DSP的最高采样电压,简直天衣无缝。

2AD823的低供电电压:使用在功耗要求非常苛刻的微型并网逆变器上最合适不过了,对该芯片采用3.3V的电压供电,一方面低的供电得到低的芯片功耗,另一方面与DSP芯片的供电电压一致,减少电压路数,一举两得。

3AD823的大压摆率(22V/us):在对光伏并网逆变器的输出交流电压、电流采样和放大时,产生的相位滞后也非常小,这在DSP闭环控制中,能实时采样到模拟信号尤为重要。很明显,大压摆率赋于低延时、实时控。

4AD823的低失调电压(200uV):一方面,光伏并网逆变器的输出功率是随阳光强弱变化的,当在很小的输出功率时,AD823采样到的输出交流电流也很小,因AD823低的失调电压,即使在很小的电压输入,正、负半周的幅度也非常接近。另一方面,光伏并网逆变器输出电流的直流分量也是要抑制的,以防止对含有电感类的设备(如电机)造成损坏。当因经过交流输出电流采样电路使输出的正、负半周电流的幅度不对称时,那么DSP采样正、负半周电流值得到的数字量也是高、低相差很大的,这就导致DSP控制交流输出电压的正、负半周的幅度也不对称,以致交流输出电流的直流分量增大,再且,直流分量的增大,也会使电流谐波增大。总而言之,低失调获得高对称、低谐波。

5AD823的低噪声(16 nV/Hz @ 10 kHz):在对电流小信号采样、放大时,AD823输出的电压值也相当干净,没有什么杂散噪声等干扰信号,使DSP采样更加准确。无疑,低噪声得到低干扰、低失真。

6AD823的高输入阻抗((10^13)Ω):因DSP需要采样光伏直流高压(150Vdc~500Vdc)和交流高压(185Vac~265Vac),而高压需要经过电阻与运放的输入引脚串联分压、衰减后才送给DSP,然而分压电阻阻值比较大,如果运放的输入电阻不是很大,就会造成引脚的输入偏置电流很大,以致影响到分压。为了避免运放本身的输入电阻对分压造成影响,那么运放的高输入阻抗是必须考虑的因素。即高输入阻抗带来极小的偏置电流、极小的影响分压。


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.