Post Go back to editing

ADI年度贺岁片——ADA4665-2放大器的应用

        以前基本以数字电路为主,换了工作后,逐渐增加了模拟电路的设计,但是通过在ADI的学习和了解,这些也不是什么问题了,从简单的放大器应用,到放大器的特殊应用,基本上都有所了解了。之前利用AD4665-2做了一个数据采集放大电路,其轨到轨、低功耗和最低阈值很好的解决了我的特殊问题,随后又将其应用到电压基准输出电路,更是淋漓尽致的发挥其作用,ADI的芯片的确是很给力~~~

下面是ADA4665-2的介绍:

        它是一款轨到轨输入/输出、双通道放大器,针对较低功耗预算设计进行了优化。25°C时,每个放大器的最大电源电流低至400μA;在扩展工业温度范围内,每个放大器的最大电源电流为600μA,因此该器件非常适合低功耗应用。此外,ADA4665-2具有极低的偏置电流,最大值仅为1 pA,失调电压漂移低至3 μV/°C,带宽为1.2 MHz。所有这些特性,以及5 V至16 V的宽电源电压范围,使该器件可广泛用于其它应用,包括过程控制、仪器仪表设备、缓冲和传感器前端等。此外,还提供轨到轨输入和输出摆幅,使其功能更加多样化。ADA4665-2的额定温度范围为−40°C至+125°C,提供标准SOIC和MSOP两种封装。

        在我的项目中,一方面作为模拟信号采集的信号放大器,主要利用了较宽的单电源供电,轨到轨输入特性,还有就是低功耗;第二是利用它搭建可调的电压基准输出电路,因为我的系统是4V(锂电池供电),我要输出0~10V的信号,为保证输出信号的稳定性,采用了恒压源输出调节电路,如有这方面需要的,请跟我联系~~~


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.