Post Go back to editing

2013电赛射频宽带放大器剖析(ZT)

射频宽带放大器(D题)解析



首先发挥部分包含基本要求,所以只需要设计发挥部分即可


1、电压增益大于60dB,也就是功率增益大于30dB,这个不难实现,50欧系统里面用功率增益比较方便,需要增益可调,而且没有要求步进,那么发挥余地比较大,用一片30dB的数控衰减器就行,类似产品HMC759一类,或者利用继电器与电阻自己搭一个派型衰减网络(此方法的误差较大,而且带宽会受继电器与电阻影响),宽带放大器尽量采用贴片电阻(1206,0805封装首选)。

2、输出端噪声电压测量时,一定记得要把输入短路,放大器做好屏蔽,尤其不要采用开关电源为放大器供电。

3、放大器上下限带宽可以用高阶巴特沃斯滤波器控制(不建议采用椭圆滤波器,椭圆滤波器对器件参数比较敏感),巴特沃斯滤波器边沿较为平缓,另外需要放大器大于100MHz带宽,这个自己用三极管搭就不现实了,可以采用一片集成放大器例如HMC580,ERA-3一类。带内起伏如果选择放大器合适,那么基本不需要闭环控制,1dB的起伏可以满足,闭环控制可以采用AD8307来实现对输出的幅度检测,宽带可变增益放大器可以利用AD835一类乘法器实现。或者直接调节数控衰减器实现。输出有效值大于1伏,相当于13dbm的输出,这个不难一般放大器都可以实现。

4、发挥部分5有时间可以尝试,

5、*****************有个小问题,带宽测试过程中测量的是电压增益减小3dB的带宽,但是实际都是功率减小3dB时的带宽,等同于幅度减小一半,这个有点疑问。

6、宽带放大器结构:第一级0.3M高通滤波器,利用贴片电感电容实现;第二级放大器(增益大于30dB);第三级100MHz低通滤波器;第四级程控衰减器;第五级功率检测电路

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.