Post Go back to editing

AD8331 VGA输出

你好,我在使用AD8331的时候发现,Vgain电压上升沿的时候,无信号输入,输出端也会产生一个100mV左右的波形,如果把Vgain上升边沿放缓,则输出端的波形变小,,是否因为器件本身特性如此?有没有使输出端保持平稳?

Parents
  • 想问问这个问题有没有后续了,我也遇到了同样的问题,电路基本与问题一致,DAC+运放驱动Vgain,如下图,黄色为TGC信号,红色为VGA的差分输出,使用的差分探头测试LNA无输入并且使能AD8331测试输出。在TGC基本快接近平稳后有三个尖峰脉冲。

    1、针对这个问题,我做了几个测试,断开了LNA和VGA之间的耦合电容,问题仍然存在,确定是VGA本身的问题。

    2、将Vgain固定为1V。也无此问题

    3、TGC信号再滤一次,信号上无振铃,问题依旧。

    4、所以怀疑是否是Vgain的响应时间导致,测试波形Fg45在Vgain上升到稳定前无明显的振荡

    5、用外部信号源连续波灌了50MHz 10mV的信号到AD8331,看VGA输出如同红色所示,确实响应时间非常长。但Vgain上升开始的0-200ns内,也并不是一直为零的,这些扰动能去除吗?

Reply
  • 想问问这个问题有没有后续了,我也遇到了同样的问题,电路基本与问题一致,DAC+运放驱动Vgain,如下图,黄色为TGC信号,红色为VGA的差分输出,使用的差分探头测试LNA无输入并且使能AD8331测试输出。在TGC基本快接近平稳后有三个尖峰脉冲。

    1、针对这个问题,我做了几个测试,断开了LNA和VGA之间的耦合电容,问题仍然存在,确定是VGA本身的问题。

    2、将Vgain固定为1V。也无此问题

    3、TGC信号再滤一次,信号上无振铃,问题依旧。

    4、所以怀疑是否是Vgain的响应时间导致,测试波形Fg45在Vgain上升到稳定前无明显的振荡

    5、用外部信号源连续波灌了50MHz 10mV的信号到AD8331,看VGA输出如同红色所示,确实响应时间非常长。但Vgain上升开始的0-200ns内,也并不是一直为零的,这些扰动能去除吗?

Children
No Data