MAX4940: FAQ
文档
博客
Forums
Members
Tags
Cancel
文档
MAX
MAX4940: FAQ
Created
over 8 years ago
Updated
3 months ago
Was this helpful?
Yes
No
More
Cancel
MAX4940的VDD VCC VEE VPP VNN 能同时供电吗?
对于MAX4940供电最关键的一点是VNN1和VNN2的供电电压,由于任何时候VNN1不得高于VNN2,这两个引脚的上电顺序需要特别注意。
按照MAX4940典型电路设计,当器件施加80V电源时,直接烧掉了,请问设计时需要有哪些注意事项?
如果器件上电后就烧的话,建议您检查一下电源的上电顺序以及EP的连接,根据数据手册的描述,EP必须要连接到VNN1,在上电的时候,一定要确保在任何时候VNN1<=VNN2。如果VNN1和VNN2使用同一个电源,这个就没有问题。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.