MAX44284EAUT+: FAQ

  • Created
Was this helpful?
  • MAX44284输出电压和被测电流的关系是什么?

    输出电压:Vout=Isense * Rsense*GAIN。 其中Isense为检测电流,Rsense是加在MAX 44284 正负输入间的电阻,GAIN为固定增益,根据选择芯片型号不同,有50/100/200/500 V/V.
  • 如何为检流放大器来选择合适的检流电阻?

    为检流放大器选择电阻时,通常按照下面的规则来选择: 1. 检流放大器数据手册通常会给出满量程检测电压的范围,根据实际应用中的最大电流值,留出一定的裕量来选择,比如满量程检测电压为50mV,被测量的最大电流为5A,如果考虑到电流的波动,留出10%的裕量,那么检流电阻为 50mV*(1-10%)/5A=9m ohm。 2.当电流流过检流电阻后,检流电阻会消耗一定的功率,因此在选择电阻时,要根据消耗的功率大小来选择电阻的额定功率…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.