MAX44009EDT+T: FAQ

  • Created
Was this helpful?
  • MAX44009数据处理问题

    MAX44009内部有0x03高字节流明寄存器和0x04低字节流明寄存器,如果要求精度高点的话,就可以考虑低字节的读数(和高字节一起);如果不需要的话,只考虑高字节就可以了。如果处理器资源不紧张,建议高、低字节都使用。
  • MAX44009数据手册中的总误差(Total Error)测试条件是什么?

    MAX44009数据手册中的Total Error为最大15%,其测试条件为用一个绿光(538nm)LED产生相当于的荧光灯100Lux的光强,然后测试MAX44009的输出响应。
  • 如何设置MAX44009的门限?

    该器件的门限设置方法请参考数据手册第10页。更多信息请参考数据手册第12页的“门限寄存器数据格式”部分。
  • 如何通过FIT估算MTTF

    MTTF= 1E9/FIT 如果 FIT Rate 是 0.05 @ 25C, 则 MTTF 为 1E9/0.05=2*E10 小时, 换算为年是 2.3*E6 年

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.