MAX4070ATA+: FAQ

  • Created
Was this helpful?
  • MAX4070在被测电流为0的时候,输出为什么不是理想的2.5V

    MAX4070内部具有2.5V参考源,其输出应该是 VOUT = 2.5V + RSENSE * ISENSE * AV,所以当 ISENSE = 0 的时候,VOUT应该是2.5V。 但是请注意MAX4070有输入范围的要求,差模输入在+/-0.3V之内,共模输入在1.35V至24V之内。也就是说,对于RS+和RS-两个引脚,每个脚的对地电压都要在1.35V至24V之内,这两个脚之间的压差在+…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.