在MAX4063的推荐电路图中,为什么在输入端要使用0.1uF的电容,而在输出端使用1uF电容?
文档
博客
Forums
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
8 months ago
文档
MAX
MAX4063: FAQ
在MAX4063的推荐电路图中,为什么在输入端要使用0.1uF的电容,而在输出端使用1uF电容?
对于输入电容,有两个作用:1.隔离直流电压。2.构成高通滤波器。该输入电容值可以从0.1uF至10uF选择,0.1uF可以提供很好的低频滤波器,较大电容有助于器件的CMRR特性。因此在数据手册中的典型应用电路图采用了0.1uF的电容,在评估板上采用了10uF的输入电容。对于输出电容,对于大多数应用可以选择1uF。
MAX4063
000098534
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.