MAX2616: FAQ
文档
博客
Forums
Members
Tags
Cancel
文档
MAX
MAX2616: FAQ
Created
over 8 years ago
Updated
3 months ago
Was this helpful?
Yes
No
More
Cancel
MAX2616在1 GHz以下的1dB压缩点(OP1dB)是多少?
MAX2616数据手册仅规定了1 GHz或更高频率下的OP1dB,使用MAX2616EVKIT对40 MHz至1 GHz进行S21测量。选择-20dBm至+2dBm的输入功率,步长1dBm。输入功率为-20dBm时,在1 GHz下测得的S21为18.18dBm,与数据手册规定的18.4dBm (典型值)非常接近。 输入功率为0dBm至1dBm时,扫描中多数频率下的增益存在1dB下降。1 GHz下的实测OP1dB…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.