Article MAX2066 不用rapid-fire功能时,STATE_A和STATE_B如何连接?

MAX2066的衰减“增益”是通过并口D0-D4 (引脚11-15)或串口SPI (配合STATE_A、STATE_B)配置。

  1. 如果使用并口配置,则将SER/PAR引脚置0;STATE_A = 0, STATE_B = 0可任意置“0”或“1”;

 

  1. 如果使用串口配置,则通过SPI接口写入28位数据(包括d0-d7 = 0保留位,Digital Attenuator State 1,Digital Attenuator State 2,Digital Attenuator State 3, Digital Attenuator State 4 )即可。其中Digital Attenuator State_对应于STATE_A、STATE_B的状态选择配置。由此可以看出,每次SPI写操作可以配置4个衰减值(或4个状态),而STATE_决定了最终的衰减值。如果您不需要切换STAEE_A和STATE_B,则将2个引脚接固定状态,比如STATE_A = 0, STATE_B = 0,则说明增益值选定的是State 1,对应于SPI数据的D8 -D12,其余三个状态值随意。

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.