AD9x
文档
博客
Forums
Members
Tags
Cancel
文档
AD9x
Created
2 months ago
Was this helpful?
Yes
No
More
Cancel
[征文原创]AD9739使用的经验分享1
[征文原创]AD9739使用的经验分享1 by shane AD9739 使用经验分享 -- 张亢 6523.attachments.zip
AD9523-1_仅使用PLL2
是否可以旁路AD9523-1的PLL1,直接在OSC引脚输入一个参考时钟? 在数据手册中,我没有找到任何可以禁用PLL1的寄存器,因此我不确定是否可以将其旁路。
AD9551_基准输入规格
数据手册中说,单端输入的最低输入电压为250mVpp。但它没有说明最大值。数据手册也没有给出建议的输入驱动电路。我想知道,对于单端基准输入,是否可以将/refx直接连接到GND?
AD9838_相位噪声
有一个客户想要利用AD9838 DDS产生96KHz/443KHz频率,预期相位噪声为-110dBc/Hz @ 10KHz。 使用10MHz MCLK和-155dBc @ 10KHz可以获得多少相位噪声? DDS是分频器件,如果只考虑参考时钟的噪声,相位噪声性能可以提高20log(fclk/fout) dB。 但事实上,AD9838会增加总噪声,我无法预测,因为数据手册未给出AD9838的残余相位噪声…
AD9880_SA0引脚
有一个关于AD9880 I2C地址的问题。 数据手册第10页上说I2C地址为0x98。但第56页上有不同的说明。I2C地址似乎可以通过SA0输入引脚改变。 但我找不到关于SA0引脚的任何说明。 您能否确认AD9880只有一类I2C地址。另外,烦请告知“由SA0输入引脚的状态设置”是什么意思?
AD9880AD9398_HDCP加密软件
如何向ADI公司申请HDCP密钥? Attachments: AD9880AD9398_HDCPencryptsoftware.zip
AD9882_HDCP检测
使用AD9882时,它能自动解密输入的HDCP信号。 另外,此芯片也能处理普通非HDCP信号。问题是,对于AD9882,如何知道输入信号是否是HDCP? 如何使用i2c寄存器来读取这些信息?
AD9910_相位噪声2
还有一位客户,他测试AD9910后指出:当并行数据端口使能且数据目的地为相位时,输出频率主要由FTW寄存器(地址0x07)决定,这与数据手册所述不相符。 有些DDS,例如AD9958和AD9959,其数据手册提供的相位噪声性能以外部参考时钟频率等于500 MSPS为条件,但没有提供参考时钟的相位噪声性能。我认为,参考时钟与输出频率的相位噪声和杂散特性之间存在某种关系。假设参考频率为fref,输出频率为fout…
AD9910_相位截断位
AD9910有多少位被截断?我想计算相位截断导致的失真。
AD9981与AD80105Z的区别
AD9981与AD80105Z有何区别
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.