AD7x
文档
博客
Forums
Members
Tags
Cancel
文档
AD7x
Created
2 months ago
Was this helpful?
Yes
No
More
Cancel
AD711_PDIP封装引脚8连接
是否可以将AD711引脚8(NC引脚)接地?
AD7190_2倍增益和4倍增益设置
我查看了AD7190数据手册的增益。为什么001和010被保留,无法设置2倍和4倍增益?恳请澄清,先行感谢!
AD7190_AINCOM范围
下面是AD7708的AINCOM范围限值。但对于AD7190,我找不到关于AINCOM范围的类似参数。能否请您提供此数据?
ad7190_内部时钟上电时间
在单次转换模式下,AD7190的片内振荡器上电大约需要1 ms。如果客户使用外部晶振或时钟,器件是否仍然需要上电时间?如果需要,上电时间是多少?
AD7192输入范围
我想请您确认AD7192是否可以设置2倍和4倍增益。 我发现下列寄存器的2倍和4倍增益设置被保留。 但在双极性/单极性配置部分,提到可以设置2倍增益。恳请确认! Attachments: FWAD7192inputrange.docx
AD7323的输出码
我的问题是: 1. 如果输入范围是0~+10V,编码为二进制补码,那么当输入为0V时,符号位是什么,其余12位是什么?另外,当输入为+10V时,符号位是什么,其余12位是什么? 2. 如果输入范围是-10V~+10V,编码为二进制补码,那么当输入为-10V时,符号位是什么,其余12位是什么?另外,当输入为+10V时,符号位是什么,其余12位是什么? Attachments:
AD736ARZ结温
请帮助提供AD736ARZ的结温,数据手册中未说明。结温与存储温度相同吗?
AD7606的关断和待机模式
在关断模式下工作时,输出引脚异常,直流功耗大于其它模式。DB7:高电平(5V);BUSY:高电平;/CS:高电平;直流功耗大于100mA。我使用HOST进入关断模式,然后让AD7606上电。 Attachments:
AD7606的输入悬空
对于AD7606,当输入引脚(V1~V8)悬空且V1GND~V8GND接地时,数字输出约为6600;如果使用万用表测量V1-V1GND,电压约为1.8V。这是正常现象吗?另外,如果V1和V1GND均连接到GND,则ADC结果为0。
AD7656与AD7656-1的区别
AD7656和AD7656-1的输入结构有何区别? 或者: A) 如果AD7656和AD7656-1的输入通过100kohm电阻连接到AGND,这两款器件有何区别? B) 如果AD7656和AD7656-1的输入直接连接到AGND,这两款器件有何区别? Attachments: AD7656_DifferencebetweenAD7656andAD7656-1…
>
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.