AD5x

  • Created
Was this helpful?
  • AD5420_引脚5连接

    1.能否解释一下下图1 AD5422 EVB中R27插口的作用? 2.对于AD5420,如下图2所示,第1、第11和第12个引脚是AGND,第4个引脚是DGND。第5个引脚呢? Attachments: AD5420_pin5connection.docx
  • ad5421_两个器件共享一个SPI

    客户使用2片AD5421并希望它们共享同一SPI总线,因而将两个SDI连在一起,并将两个SDO连在一起。 客户可以正确写入这两个AD5421,但读取时遇到一些问题。详细测试方法如下所述。 我查阅了数据手册有关AD5421 SPI接口的内容,它没有“CS”引脚来使能/禁用SPI。因此,我无法确定SYNC引脚能否用作“CS”来禁用未使用的器件。如果不能,是否意味着两个AD5421无法共享同一SPI总线…
  • AD5446_SFDR

    1. 在AD5446数据手册中,只有fout=50KHz和20KHz下有一个SFDR规格。而fout=500KHz下则没有。我还查看了AD5449数据手册,它在500KHz fout下提供了此规格。如果有的话,能否提供AD5446在500KHz下的SFDR?或者,能否就以下要求给出一些器件选型建议:500KHz fout下的SFDR大于70dB、分辨率为14/16位、Fs>1MHz? AD5446…
  • 数字电位计_带宽

    我检查了几款电位计,带宽全都小于1MHz。 我们是否有带宽达到10 MHz的电位计产品?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.