博客
Forums
Members
Tags
Cancel
文档
AD1x
AD5x
AD6x
AD7x
AD8x
AD9x
ADA
ADIS
ADL
ADV
CN
General
MAX
More
Cancel
Recently Updated Articles
最爱ADI放大器之- AD712
最爱ADI放大器之- AD712 by huangguimin 我最喜欢的ADI放大器AD712是一款 双通道、 高速、精密、单芯片运算放大器,具有极高的性价比。我是玩音响的,也就是玩HIFI的,我用这颗运放作为整个HIFI功放的输入前端,也就是前级。运放对选型对整个功放的素质影响很大,不同的运放能产生天壤之别的音质差异。对这颗运放比较熟悉,整体来说AD712是不错的运放!属于监听级的类型。特显中频与高频之间的过度交替。声场比较广!低音稍少!高音稍粗(相对高级的)低噪音很静没有半点杂音。听纯音乐女声不错属于比较耐听的运放之一…
最爱放大器之-AD8138
最爱放大器之-AD8138 by xxff622 AD8138 -- 使用过的第一款ADI的运算放大器! 应用:使用在 CMMB数字电视接收机中。 用途:作为AD9203的单端转差分的输入buffer,把单端的低中频IQ信号变为差分。同时提供适合的直流偏置给AD9203。 特点:320M的高带宽以及 5 nV/√Hz的噪声参数完全胜任此工作,同时具有Vcom引脚,方便的设置共模电压。
AD5420_引脚5连接
1.能否解释一下下图1 AD5422 EVB中R27插口的作用? 2.对于AD5420,如下图2所示,第1、第11和第12个引脚是AGND,第4个引脚是DGND。第5个引脚呢? Attachments: AD5420_pin5connection.docx
AMP03: 高速差分放大器
AMP03: High Speed Differential Amplifier by zrk787 AMP03: High Speed Differential Amplifier The AMP03 is a single-chip, unity-gain, high-speed differential amplifier with a matched thin-film resistor network that operates stably over the entire…
ADI院士访谈:如何用先进模拟技术打造完美音效
ADI Academician Interview: How to Create Perfect Sound with Advanced Analog Technology by ADI_Amy This article is the "Electronic Engineering Album" reporter Shao Lefeng interviewed by ADI academician Scott Wurcer (original "using advanced analog technology…
Most Helpful Articles
[ADI微博问答精选] 请ADI介绍些跨导型运放的学习资料
[ADI microblogging question and answer selection] Please introduce some learning materials of transconductance op amps by ADI by ADIForum @ 黑和白的精彩 : This LED chip is said to be a transconductance op amp inside. Usually I contact more current type and…
[ADI微博问答精选]请教关于三运放仪用放大器芯片AD8421的问题
[ADI微博问答精选]请教关于三运放仪用放大器芯片AD8421的问题 by ADIForum @ 陳子建 Wonder : 请问大神,对于三运放仪用放大器芯片 AD8421 ,把它用于第二级放大的时候,前一级的两个放大器输出的共模电压达到 AD8421 的工作电源的时候, AD8421 是不是很容易就饱和了? ADI 专家: AD8421 的三运放架构在消除差动放大器级的共模电压之前,在第一级调节增益。第一级与第二级间的内部节点 ( 图 61 中的节点 1 和 2) 上的信号是由增益信号…
[征文] 关于仪运放AD620的原理及计算(原创)
[Essay] About the principle and calculation of the instrument AD820 (original) by shane Into the company, to design a strain for small signal amplification product, as it relates to some of the differential amplifier, by selecting the multi-comparison…
[征文原创]AD9739使用的经验分享1
[征文原创]AD9739使用的经验分享1 by shane AD9739 使用经验分享 -- 张亢 6523.attachments.zip
【CN0151】利用DAC、运算放大器和MOSFET构建可编程电流源
[CN0151] Build a programmable current source with DAC, op amp, and MOSFET by zrk787 [CN0151] Build a programmable current source using DACs, operational amplifiers, and MOSFETs Circuit function and advantage Digitally controlled current sources…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.