Post Go back to editing

EVAL-ADICUP3029 使用CCES3.03无法debug,U盘模式上次bin或Hex也不运行

Thread Summary

The user encountered issues running hello world and blinky_example programs on the ADuCM302x using CCES 3.03 and OpenOCD 0.12.0, with the green and blue LEDs remaining constantly lit. The problem was resolved by using CCES 2.11 and OpenOCD 0.10.0, and modifying the aducm302x.tcl and aducm3029.cfg files according to the error messages.
AI Generated Content

我用的CCES 3.03,使用包里自带的hello word 和 blinky_example程序都试过了,用bin和hex 文件拷贝到开发板U盘模式绿灯和蓝灯一直常亮,程序没运行,不知道哪的问题? 用CMSIS-DAP模式debug,而且试了好几个版本的ADuCM302x_DFP差不多都是一样的结果,错误如下:用通义修改错误很多次仍然解决不了问题

Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0) OpenOCD 0.12.0 (2025-04-03-09:09)
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
0
DEPRECATED! use 'adapter speed' not 'adapter_khz'
D:/analog/cces/3.0.3/ARM/packs/AnalogDevices/ADuCM302x_DFP/3.2.1/openocd/scripts//target/aducm302x.tcl:55: Error: target requires -dap parameter instead of -chain-position!
in procedure 'script'
at file "embedded:startup.tcl", line 28
at file "D:/analog/cces/3.0.3/ARM/packs/AnalogDevices/ADuCM302x_DFP/3.2.1/openocd/scripts/target/aducm3029.cfg", line 6
at file "D:/analog/cces/3.0.3/ARM/packs/AnalogDevices/ADuCM302x_DFP/3.2.1/openocd/scripts//target/aducm302x.tcl", line 55

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.