Post Go back to editing

aducm360的复位电路RST引脚怎么接

1.硬件:按照EVAL的电路图,RST是连到仿真器DAP上,使用SWD方式连接,但是RST未接电容和电阻。

2.现象:开始是可以正常工作。 后来在AV3.3V上接了两个分压电阻10K到地,分压出1.65V,此时,就无法正常复位了。

3.测试:断电长时间后(彻底断电),再上电,不能正常工作,若是断电后立刻上电,就可以正常。不知道是不是复位电路问题呢? 查看论坛,飞线了插针电阻5.1K和插针电容0.1uf,仍然是这个问题。

Parents
  • 你好,

    1. 按照评估板的电路连接是没有问题的,ADuCM360有内部上拉,所以外部上拉电阻可以不接,滤波电容如果你有需要可以接上。

    2. 请问你分压1.65V是什么目的?这个1.65V是接到了什么位置?

    3. 按照你2中的描述,是电路已经不正常工作了,建议你按照评估板推荐的电路,如果还有疑问请把你的问题以及目的描述清楚,电路图附上,我们看一下。

    Jon

  • 1分压1.65V是用来给后面的放大器提供基准电压用。

    2另外还有一些问题,焊接到i-v转换的ADA4627后电流明显增大,增加了70mA,焊接仪表放大器ad8253电流明显增大,增加了40mA。不知道是哪有问题的

Reply Children
No Data