Post Go back to editing

新手咨询ADUC7020 PWM问题

我想用ADUC7020产生三路PWM,并输出,但是7020能配置成PWM的管教只有P3.0-P3.7,按我的理解,PLA的  block2产生三路PWM,一路通过PLA block2 的ELEMENT15引到block1的 P0.4,P0.5,P0.6,P0.7,P1.7,P2.0中的某一个IO口输出), 一路通过PLA block2 的P4.2输出,第三路不知道怎么输出了?

Parents
  • 您好,感谢你的回复,你的附件我已看到,可能您没理解我的问题,PWM配置我会,不会的是输出引脚配置这块,aduc7024/25/26/27/28/29由于存在P3.0-P3.7口,所以PWM输出不存在问题,但是aduc7019/20/21/22不存在P3.0-P3.7口,所以PWM输出必须通过PLA引到其他IO(支持PLA)输出,我的问题就是有两路PWM可以引出到其他IO并输出,第三路不知道如何引到其他IO!

Reply
  • 您好,感谢你的回复,你的附件我已看到,可能您没理解我的问题,PWM配置我会,不会的是输出引脚配置这块,aduc7024/25/26/27/28/29由于存在P3.0-P3.7口,所以PWM输出不存在问题,但是aduc7019/20/21/22不存在P3.0-P3.7口,所以PWM输出必须通过PLA引到其他IO(支持PLA)输出,我的问题就是有两路PWM可以引出到其他IO并输出,第三路不知道如何引到其他IO!

Children
No Data