Post Go back to editing

ADUCM360的ADC

目前正在使用ADuCM360BCPZ128芯片的AD采集模块,不太会用,我想用AD采集模块采集外围电路上的电压,需要连续采集,请问硬件上该怎么连接啊? 就如下图,我想采集R1上的电压值,R2是个滑动变阻器,R1两端电压在0-30V之间变化,请问:ADC内部参考电压(1.2V)和外部参考电压(2.5V),选哪个?是否需要连接VREF+和VREF-?需要在AIN0,AIN1与外围电路之间添加降压网络吗,因为30V挺大的。