1. 如果ADC使用单端模式,在寄存器ADC0CON中有这样的描述,“Note that single-ended channels are selected with respect to ADC5. Bias ADC5 to a minimum level of 0.1 V.”,这是为什么?
2. 如果ADC4输入0.01V直流,ADC5 = 0.2V,那对ADC4单端测试的结果是多少?
3. ADuC7060对几mV的小信号,进行单端测试,是否可能不准?我做过测试,两块ADuC7060同时用ADC4测试一个电压,都设置ADC5=0。当ADC4变化时,一块板测试结果从0.5mV变化到1mV,另一块板的测试结果从0.3mV到1.8mV,补充:两块板ADC的MMR配置完全相同。