English
EngineerZone
ADUC Cortex M3系列
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
ADUC Cortex M3系列
Cancel
ADUC Cortex M3系列
问答
讨论
文档
成员
标签
Cancel
Need Help? Ask a Question
This group hosts discussions and FAQs regarding ADUC Cortex M3系列. Please read the Analog Devices EngineerZone
Code of Conduct
before posting.
All Threads
by
AndyLi24
ADUC Cortex M3系列
Latest
8 months ago
by
Kx3
591
2
0
Not Answered
调试接口无法访问
0
Not Answered
在MDK中开发了aducm330的程序,基于官方例程的设置,刷写编译后的程序到板子以后,板子的调试接口便无法访问。 出现如下的错误: 是什么原因导致的?如何进行修复?
software
microcontrollers
Precision Microcontrollers
aducm330
591
2
0
by
YCD
ADUC Cortex M3系列
Latest
over 1 year ago
by
mashimaro
586
2
0
Not Answered
EVAL-ADICUP360 + EVAL-CN0338-ARDZ 不能正常工作
0
Not Answered
EVAL-ADICUP360 + EVAL-CN0338-ARDZ 不能正常工作,畫面上有出現mbed serial port但下載的ADuCM360_demo_cn0338.bin 拖曳到MBED磁碟,都無法燒錄 請問該如何排查問題
software
CrossCore Embedded Studio 2.12.1
eval-adicup360
586
2
0
by
LeeVise
ADUC Cortex M3系列
Latest
over 1 year ago
by
mashimaro
478
1
0
Not Answered
ADICUP360 usb debug driver
0
Not Answered
Hi, I use the ADICUP360 demo board connect to my PC, but this demo kit's driver is not work. Microsoft.DeviceManager displays a error that the demo kti's usb port was indentified "UCM-UCSI ACPI DEVICE". pls help me to solve it ! thanks a lot
software
adicup360
CCES 2.12.1
ADMCU360
UCM-UCSI ACPI DEVICE
Show More
478
1
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1306
3
0
Answered
如何对ADuCM360/1进行功耗优化?
0
Answered
ADuCM360/1是针对低功耗的应用,能否详细介绍一下在实际设计时如何进行功耗优化?
aducm360/1
1306
3
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1235
2
0
Answered
请问ADuCM360中的两个ADC能否支持同步采样?
0
Answered
请问ADuCM360中的两个ADC能否支持同步采样?
microcontrollers
Precision Microcontrollers
aducm360
1235
2
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1181
2
0
Answered
ADuCM360/1可否通过XTALO/XTALI引脚外接时钟?
0
Answered
我有一个要求时序非常精确的应用。可以将一个 16.0000 MHz 晶体连接到 XTALO/XTALI 引脚 , 并利用它来为 Cortex M3 内核提供时钟吗 ? 如果行 , 您能推荐内部振荡器通常需要的分立元件值 ( 电阻 R 接在晶体两端 , 电容 C 从晶体的一侧连接到地 ) 吗 ?
aducm360/1
1181
2
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1091
2
0
Answered
请问哪里可以获得关于AduCM360/1寄存器的信息?
0
Answered
请问哪里可以获得关于AduCM360/1寄存器的信息?
aducm360/1
1091
2
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1156
2
0
Answered
基于ARM7的ADuC器件上仿真器能否支持调试基于Cortex-M3的ADuC器件?
0
Answered
在基于 ARM7 的 ADuC 器件上 , 通过 JTAG 调试和下载到 Flash 。在 AduCM360 上 , JTAG 被串行线调试取代。 串行线调试与 JTAG 有何区别 ? 我是否需要新的工具和新的仿真器 ?
aducm360/1
1156
2
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1129
2
0
Answered
ADuCM360/1是否支持存储器到存储器DMA传输?
0
Answered
ADuCM360/1是否支持存储器到存储器DMA传输?
aducm360/1
1129
2
0
by
BruceLuo
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1430
2
0
Answered
您能就ADuCM360/1中的SINC3和SINC4数字滤波器性能与不同ADC采样速率之间的关系提供更多信息吗?
0
Answered
您能就ADuCM360/1中的SINC3和SINC4数字滤波器性能与不同ADC采样速率之间的关系提供更多信息吗?
aducm360/1
1430
2
0
View All Threads
by
李华贵
ADUC Cortex M3系列
Latest
over 8 years ago
by
barryzhang
1212
1
0
Answered
ADUCM361独立PWM怎么配置?
0
Answered
在一个仪表应用中,ADUCM361口线分配完成发现需要2个独立的PWM信号,口线只剩如下两个: P1.2/PWM0/RI P1.3/PWM1/DSR 但手册UG_367中page164有 注意:每个通道的高端PWM输出的高电平持续时间必须大于或等于低端输出的高电平持续时间。 例如,PWM0的高电平周期必须等于或大于PWM1的高电平周期。 标准模式(非H桥模式)不能各自输出正脉冲可变宽度的信号??? 实验了一下: #define PWMPERIOD 0x9C40 /...
aducm361独立pwm怎么配置
1212
1
0
by
RyanHsiung
ADUC Cortex M3系列
Latest
over 9 years ago
by
hpkamen
960
1
0
Answered
CM3WSD源码
0
Answered
现360已经批量使用,准备基于现有的CM3WSD串口升级来开发一个我自己的以太网升级设备软件。 上位机是以太网,下面有网关实现以太网转串口,并来控制BOOT RST 1、CM3WSD。exe有源码吗?? 2、若没有源码,下位的的再线升级的固件有开放源码吗、 3、若上面两个都没有,有具体的操作流程祥解吗? analogchina-admin hdx2 Analog1
960
1
0
by
bomlulu
ADUC Cortex M3系列
Latest
over 10 years ago
by
bomlulu
1414
2
0
Answered
ADUCM360:如何用外部中断将CPU从睡眠模式唤醒?
0
Answered
需要实现的功能:ADUCM360外接时钟,时钟定时中断引脚连接CPU的外部中断6,CPU不工作时进入睡眠模式,当时钟定时到达5分钟时,外部中断将CPU从睡眠模式唤醒,并执行一些测量运算,完成后继续进入睡眠模式,周而复始。 代码都是利用EVLES提供的库函数代码。 进入睡眠模式的代码如下: PwrCfg(PWRMOD_MOD_TOTALHALT); 外部中断设置如下: EiCfg(EXTINT6,INT_EN,INT_RISE);//外部中断6,P1.6使能,上升沿触发 ...
microcontrollers
Precision Microcontrollers
aducm360
1414
2
0
by
ruohua
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
2933
5
0
Answered
ADUCM320 MDIO口使用问题
0
Answered
1.ADUCM320 MDIO口的电平是多少? 是1.2V的么?还是1.8V? 3.3V? PRTADR/MDIO/MDC可直接和CFP接口的MDIO口连接 通信么? 2.通过 MDIO进行烧录程序时,BM引脚是否要拉低? 然后在320正常工作时候要拉高? 3. ADUCM320是否可以作为主机 通过MDIO口控制其他的从机, MDIO/MDC作为总线?
aducm320 mdio
microcontrollers
aducm320
Precision Microcontrollers
2933
5
0
by
maxihecker
ADUC Cortex M3系列
Latest
over 7 years ago
by
EZAdministrator
1634
2
0
Answered
请教关于aduc7027 PWM问题
0
Answered
目前项目中需要通过aduc7027的PWM1L对应端口产生如下脉冲波形,频率固定为43K左右,占空比为在200个周波内从0~1间呈正弦波形式变化。 目前问题,43Khz方波输出正常,想通过PWM_SYNC中断去调节占空比,但貌似从PWM1L只能输出占空比低于1/2的波形,而且不太明白为什么PWM_SYNC的中断频率不是43K,而是远大于43K。
microcontrollers
ARM7 Core Products
aduc7027
pwm
1634
2
0
by
zhanmia
ADUC Cortex M3系列
Latest
over 10 years ago
by
ADI_XUN
2428
7
0
Answered
ADUCM320的复位电路
0
Answered
请问如果不使用开关,不使用复位芯片,如何设计ADUCM320的上电复位电路?我用传统的RC(10k&10uF)复位方法做不出来。
microcontrollers
aducm320
Precision Microcontrollers
2428
7
0
by
zhanmia
ADUC Cortex M3系列
Latest
over 11 years ago
by
hpkamen
897
1
0
Answered
ADUCM320的低功耗应用
0
Answered
我在使用ADUCM320做高性能、低功耗系统的设计,IDAC用不到,能不能悬空它的供电脚PVDD以降低功耗?麻烦各位专家帮我解答。
microcontrollers
aducm320
Precision Microcontrollers
897
1
0
by
chenxiaoli
ADUC Cortex M3系列
Latest
over 11 years ago
by
ADI_XUN
566
1
0
Answered
关于Keil uVision4 里面如何添加ADucM360型号的问题
0
Answered
你好,我安装了正版Keil uVision4 ,建工程时,选择CPU型号时,没有ADUCM360,有ADUC7xxx系列 ,请问如何添加?
microcontrollers
Precision Microcontrollers
aducm360
566
1
0
by
tlijun
ADUC Cortex M3系列
Latest
over 11 years ago
by
ADI_XUN
2571
5
0
Answered
使用ADUCM360过程中的问题
0
Answered
使用ADUCM开发过程中遇到如下问题: 开发环境:KEIL FOR ARM V4.70,JLINK V8.0 V4.59d驱动 问题1: 使用程序:example 里面的 Blink程序 问题描述:用JLINK可以正常仿真下载,第一次脱离JLINK可以正常运行;但是,如果程序下载完成之后重新上电后,芯片将不再运行。 附件是原理图和JLINK配置图。 问题2: 使用程序:example中的Timers 问题描述:用jlink仿真时,在GP_Tmr0_Int_Handler...
cortex-m3
microcontrollers
Precision Microcontrollers
aducm360
2571
5
0
by
chenxiaoli
ADUC Cortex M3系列
Latest
over 11 years ago
by
ADI_XUN
1500
3
0
Answered
关于应用笔记CN0319
0
Answered
应用笔记中有以下电路: 见附件1 谁能讲讲这个电路的原理 如何得出R12 处的电压的?? 笔记上说R12=(Vrloop+Vref)*R2/(R1+R2)-Vrloop
cn0319
1500
3
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More