讨论
文档
Members
Tags
Cancel
常见问题
马上提问
Open Questions. Can you
help
?
调试接口无法访问
Not Answered
11 months ago
固件烧录进去不运行
Not Answered
over 1 year ago
EVAL-ADICUP360 + EVAL-CN0338-ARDZ 不能正常工作
Not Answered
over 1 year ago
ADICUP360 usb debug driver
Not Answered
over 1 year ago
在keil环境下,使用ADuC官方ADuC706x的demo,用jlink调试,程序无法从main开始运行
Not Answered
over 1 year ago
该专区内容有关ADUC微处理器专区的讨论和常见问题解答。 发帖前请阅读 Analog Devices EngineerZone 行为准则。
All Threads
by
douxiangdong
ADUC微处理器专区
Latest
3 months ago
by
hjj861
2149
3
0
Answered
aducm360串口通信可以发送但是不能接收
+1
Answered
aducm360 向PC发送没有问题,但是PC向主板发送时不产生接收中断,不知是为什么 串口初始化,和是断服务例程,串口中断有打开,打开的语句在系统初始化里面,请帮我看看是那里的问题 void UART_Int_Handler () { volatile unsigned char ucCOMSTA0 = 0 ; volatile unsigned char ucCOMIID0 = 0 ; ucCOMIID0 = UrtIntSta (pADI_UART); if...
microcontrollers
Precision Microcontrollers
aducm360
2149
3
0
by
pota
ADUC微处理器专区
Latest
8 months ago
by
pota
754
2
0
Answered
使用ADSP21489, 关于CCES中编程的数据sizeof(char)问题
+1
Answered
#include <sys/platform.h> #include "adi_initialize.h" #include "demo.h" /** * If you want to use command program arguments, then place them in the following string. */ char __argv_string[] = ""; int main(int argc, char *argv[]) { /** * Initialize...
adsp21489
sizeof
754
2
0
by
kiara
ADUC微处理器专区
Latest
9 months ago
by
mashimaro
841
1
0
Answered
ADuCM435
+1
Answered
ADuCM435IE是否也可以使用AN-806手册中提到I2C对flash进行擦写操作?或者是否有关于swd接口对 flash进行擦写操作的说明
software
841
1
0
by
pota
ADUC微处理器专区
Latest
10 months ago
by
YANAMIANNA
963
4
0
Answered
专家好,请问ADSP21489的DAI的IO可以路由到SPIB吗?
+1
Answered
我的主控MCU想通过SPI和ADSP21489通信,主控MCU作为SPI的主端,ADSP21489作为从端。目前DPI的IO有限,想利用DAI的IO来做SPIB的通信。请问是否可以这么设计?
963
4
0
by
AndyLi24
ADUC Cortex M3系列
Latest
11 months ago
by
Kx3
833
2
0
Not Answered
调试接口无法访问
0
Not Answered
在MDK中开发了aducm330的程序,基于官方例程的设置,刷写编译后的程序到板子以后,板子的调试接口便无法访问。 出现如下的错误: 是什么原因导致的?如何进行修复?
software
microcontrollers
Precision Microcontrollers
aducm330
833
2
0
by
sdcwhy
ADUC微处理器专区
Latest
over 1 year ago
by
sdcwhy
692
1
0
Answered
EVAL-ADICUP3029 使用CCES3.03无法debug,U盘模式上次bin或Hex也不运行
+1
Answered
我用的CCES 3.03,使用包里自带的hello word 和 blinky_example程序都试过了,用bin和hex 文件拷贝到开发板U盘模式绿灯和蓝灯一直常亮,程序没运行,不知道哪的问题? 用CMSIS-DAP模式debug,而且试了好几个版本的 ADuCM302x_DFP差不多都是一样的结果,错误如下:用通义修改错误很多次仍然解决不了问题 Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0) OpenOCD 0.12.0 (2025...
692
1
0
by
GyroZhang
ADUC微处理器专区
Latest
over 1 year ago
by
mashimaro
1058
2
0
Answered
ADuCM4050接收PCM数据问题
+1
Answered
在ADuCM4050上,使用SPORT作为音频信号PCM的接收端口,配置了BCLK为2.6MHz,LRCLK为2.6MHz,约为10kHz,时钟沿下采样,serial word length 为32位,MSB,DSP standard模式。 音频芯片按以下格式(TDM8)输出PCM数据, 使用1kHz的正弦波测试麦克风,打印接收到的数据,得到图: 接着重新配置音频芯片,按下面格式(TDM2)输出PCM数据 修改LRCLK分频为64,即BCLK 2.6MHz,LRCLK约为40kHz...
Ultra Low Power Microcontrollers
microcontrollers
aducm4050
sport
1058
2
0
by
GyroZhang
ADUC微处理器专区
Latest
over 1 year ago
by
GyroZhang
958
2
0
Answered
ADuCM4050 SPORT接口不能连续工作
+1
Answered
使用ADuCM4050作为MCU接收ADAU7002传来的PCM数据,HCLK为26MHz,BCLK为2.6MHz,LRCLK为2.6/64MHz。发现SPORT接口只在submitbuffer时产生时钟,buffer装满后,时钟就不再产生,导致麦克风芯片不在工作。能不能让sport接口一直产生时钟输出?
Video Products
Ultra Low Power Microcontrollers
microcontrollers
Sample Rate Converters
aducm4050
sport
adau7002
Show More
958
2
0
by
daviddq
ADUC微处理器专区
Latest
over 1 year ago
by
daviddq
896
2
1
Answered
The case of ADSP - 21569 (21593) uses 2 SPORTs simultaneously
0
Answered
On the 21593/21569 DVB, referring to the single SPORT Demo can run normally. When multiple SPORTs need to be used, especially when using 2 SPORTs, SPU_Init fails. I hope to provide a routine for using multiple SPORTs simultaneously.
896
2
1
by
shibinjie
ADUC8xx系列
Latest
over 1 year ago
by
mashimaro
754
1
0
Answered
aduc841定时周期如何计算
0
Answered
ADUC841,MCU外接11.0592M的晶振,不分频,目前使用ADUC841的定时器0,配置为模式1,TH0设置为0x028,TL0设置为0x00,按照理论计算定时周期应该是6s吧,实际测量是1s,请问aduc841的定时周期的正确计算方法是怎么样的?
software
microcontrollers
timer
aduc841
8052 Core Products
Show More
754
1
0
View All Threads
by
pota
ADUC微处理器专区
Latest
8 months ago
by
pota
754
2
0
Answered
使用ADSP21489, 关于CCES中编程的数据sizeof(char)问题
+1
Answered
#include <sys/platform.h> #include "adi_initialize.h" #include "demo.h" /** * If you want to use command program arguments, then place them in the following string. */ char __argv_string[] = ""; int main(int argc, char *argv[]) { /** * Initialize...
adsp21489
sizeof
754
2
0
by
kiara
ADUC微处理器专区
Latest
9 months ago
by
mashimaro
841
1
0
Answered
ADuCM435
+1
Answered
ADuCM435IE是否也可以使用AN-806手册中提到I2C对flash进行擦写操作?或者是否有关于swd接口对 flash进行擦写操作的说明
software
841
1
0
by
pota
ADUC微处理器专区
Latest
10 months ago
by
YANAMIANNA
963
4
0
Answered
专家好,请问ADSP21489的DAI的IO可以路由到SPIB吗?
+1
Answered
我的主控MCU想通过SPI和ADSP21489通信,主控MCU作为SPI的主端,ADSP21489作为从端。目前DPI的IO有限,想利用DAI的IO来做SPIB的通信。请问是否可以这么设计?
963
4
0
by
sdcwhy
ADUC微处理器专区
Latest
over 1 year ago
by
sdcwhy
692
1
0
Answered
EVAL-ADICUP3029 使用CCES3.03无法debug,U盘模式上次bin或Hex也不运行
+1
Answered
我用的CCES 3.03,使用包里自带的hello word 和 blinky_example程序都试过了,用bin和hex 文件拷贝到开发板U盘模式绿灯和蓝灯一直常亮,程序没运行,不知道哪的问题? 用CMSIS-DAP模式debug,而且试了好几个版本的 ADuCM302x_DFP差不多都是一样的结果,错误如下:用通义修改错误很多次仍然解决不了问题 Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0) OpenOCD 0.12.0 (2025...
692
1
0
by
GyroZhang
ADUC微处理器专区
Latest
over 1 year ago
by
mashimaro
1058
2
0
Answered
ADuCM4050接收PCM数据问题
+1
Answered
在ADuCM4050上,使用SPORT作为音频信号PCM的接收端口,配置了BCLK为2.6MHz,LRCLK为2.6MHz,约为10kHz,时钟沿下采样,serial word length 为32位,MSB,DSP standard模式。 音频芯片按以下格式(TDM8)输出PCM数据, 使用1kHz的正弦波测试麦克风,打印接收到的数据,得到图: 接着重新配置音频芯片,按下面格式(TDM2)输出PCM数据 修改LRCLK分频为64,即BCLK 2.6MHz,LRCLK约为40kHz...
Ultra Low Power Microcontrollers
microcontrollers
aducm4050
sport
1058
2
0
by
GyroZhang
ADUC微处理器专区
Latest
over 1 year ago
by
GyroZhang
958
2
0
Answered
ADuCM4050 SPORT接口不能连续工作
+1
Answered
使用ADuCM4050作为MCU接收ADAU7002传来的PCM数据,HCLK为26MHz,BCLK为2.6MHz,LRCLK为2.6/64MHz。发现SPORT接口只在submitbuffer时产生时钟,buffer装满后,时钟就不再产生,导致麦克风芯片不在工作。能不能让sport接口一直产生时钟输出?
Video Products
Ultra Low Power Microcontrollers
microcontrollers
Sample Rate Converters
aducm4050
sport
adau7002
Show More
958
2
0
by
daviddq
ADUC微处理器专区
Latest
over 1 year ago
by
daviddq
896
2
1
Answered
The case of ADSP - 21569 (21593) uses 2 SPORTs simultaneously
0
Answered
On the 21593/21569 DVB, referring to the single SPORT Demo can run normally. When multiple SPORTs need to be used, especially when using 2 SPORTs, SPU_Init fails. I hope to provide a routine for using multiple SPORTs simultaneously.
896
2
1
by
shibinjie
ADUC8xx系列
Latest
over 1 year ago
by
mashimaro
754
1
0
Answered
aduc841定时周期如何计算
0
Answered
ADUC841,MCU外接11.0592M的晶振,不分频,目前使用ADUC841的定时器0,配置为模式1,TH0设置为0x028,TL0设置为0x00,按照理论计算定时周期应该是6s吧,实际测量是1s,请问aduc841的定时周期的正确计算方法是怎么样的?
software
microcontrollers
timer
aduc841
8052 Core Products
Show More
754
1
0
by
RICYN
ADUC微处理器专区
Latest
over 2 years ago
by
mashimaro
1374
1
0
Answered
ADUC7023BCPZ62I date code marking 问题
0
Answered
您好,请帮忙看看这个芯片的date code怎么看,具体是哪年那周的?感谢!
1374
1
0
by
SWAST
ADUC微处理器专区
Latest
over 2 years ago
by
mashimaro
1085
1
0
Answered
aduc系列串口保护
0
Answered
您好,我们经常使用ADuc834,但是经常出现一个问题. 第一个问题是:WSD无法下载程序了。 第二个问题是:不能通过串口进行通讯。我们使用的是FT232串口调试工具。经常出现和单片机无法连接的问题。 我感觉好像串口烧坏了(因为其他都不变的情况下,更换单片机又可以下载或者通讯了。)请问有没有什么好的方法,可以将ADuc的串口保护起来? 谢谢!
1085
1
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.