Post Go back to editing

ADE7880 使用单相问题

Thread Summary

The user is experiencing issues with the ADE7880 not reading correct voltage and current data. The final answer suggests that the reference voltage source was incorrectly set to 0.5V instead of the standard 1.2V, which was corrected in a hardware revision. After the revision, the user still observes non-zero VRMS values for VB and VC, which should be zero when these pins are left floating. The support engineer recommends checking the AGIAN gain register settings as a potential solution.
AI Generated Content

AD7880 读不到正确数据, 电压采样电路图如图所示va,vb,vc,vn通过分压电阻然后UAP,UBP,UCP,UN接入7880的对应电压采样引脚,

电流采样如图2所示

现在ADE7880 PM设智PM0工作模式,且往DSP寄存器写入1启动,,然后延时500ms,能够读到checksum寄存器为

0xAFFA63B9说明spi接口可用,然后UA接入开关电源火线,UN接入开关电源零线,其他UB UC管脚悬空,电流检查管脚悬空,读status1寄存器未能读到过零信号,读vrmsa,vrmsb,vrmc寄存器数值也比较奇怪,理论上应该vrmsb和vrmsc为0吧,想问下技术支持,是配置不对,还是有可能电路设计问题

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.