Post Go back to editing

MAX17205电量计如何正确配置所有寄存器

Category: Hardware

第一个问题:MAX17205 用EZ配置电池相关参数,但我发现Empty Voltage最低只能设置为3V,我想设置成2.5V或2.4V有办法实现吗?

第二个问题:我看MAX17205芯片手册,有好多寄存器,许多寄存器都不理解什么意思,我该如何配置它们?哪些寄存器是必须配置的,哪些可以使用默认参数?

  • 1.MAX17205针对部分电池内部有对应的电量算法,您使用内置算法时,最低电压的设置范围是固定的。如果您需要设置成更低的Emoty Voltage,可以尝试更换电池的类型或重新建立电池模型和电量算法。

    2.该部分的寄存器是需要您自己根据需求进行配置的,不同类型的电池和需求,配置的寄存器也是不同的。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.