Post Go back to editing

MAX17205电量显示异常

2S电池组电量计选用的是MAX17205,经过几轮充放电(电池浮充)后出现容量显示异常问题。 问题现象:电池充满后贮存15天发现容量变为1%,但是电压仍是8.2V。通过MAX1720X上位机与电池通讯发现有一个-20mA的静态电流。 将电量计重置后,静态电流消失了,容量回复正常。 实验复现:复位后再次经过几轮充放电循环后,用上位机记录数据,发现IC的Status(6c:00)寄存器值由0X0080变为了0X4080,然后就出现了-20mA的静态电流。 通过查阅芯片手册,好像是Status寄存器中Smx被置位(Maximum SOC Alert Threshold Exceeded. This bit is set to a 1 whenever SOC rises above the maximum SAlrtTh value) 问题一: (Maximum SOC Alert Threshold Exceeded. This bit is set to a 1 whenever SOC rises above the maximum SAlrtTh value)这句话是说SOC超过了最大阈值吗? 问题二: 最大SOC阈值是根据SAlrtTh寄存器(芯片手册Figure 61. SAlrtTh (003h)/nSAlrtTh (1C2h) Format)设置的,我的至是FF00,转换成10进制是多少? 问题三: Status(6c:00)寄存器变为0X4080为什么会有假电流?