Post Go back to editing

LTC6811-1

Hello to ADI support team ,

 I have some questions according LTC6811-1 . I use cascade connection of two LTC6811 for 20S cells connection .

1.  I have mode in with  Controller is disconnected and  both LTC6811-1 operating without external Controller .

          1.1    Is it possible  disable Balancing mode by HW with signal to  pin  in this mode ?

          1.2    Does  both LTC's in sleep in this mode ?

B.R

Alex Burtakov

Parents
  • Please check the "WATCHDOG AND DISCHARGE TIMER" section in datasheet page 35. IC will go to sleep if Watchdog timer expires. But there is an exception when Discharge timer is enabled and the Discharge Timeout duration is selected (DCTO) then you can disconnect controller for the duration set by DCTO. once that expires IC will go to sleep, so you need to make any communication before DCTO expires. 

Reply
  • Please check the "WATCHDOG AND DISCHARGE TIMER" section in datasheet page 35. IC will go to sleep if Watchdog timer expires. But there is an exception when Discharge timer is enabled and the Discharge Timeout duration is selected (DCTO) then you can disconnect controller for the duration set by DCTO. once that expires IC will go to sleep, so you need to make any communication before DCTO expires. 

Children
No Data