问答
讨论
文档
Members
Tags
Cancel
常见问题
马上提问
Open Questions. Can you
help
?
Regarding Power Factor and Power Measurement Accuracy Using CT on CT Secondary with ADE7880
Not Answered
2 months ago
ADE7858 无法输出CF
Not Answered
3 months ago
ADE7913测试ADC输出码的标称值差异较大
Not Answered
5 months ago
LTC2959IDDB#TRPBF芯片电流误差为10%
Not Answered
6 months ago
AD9525配置问题
Not Answered
6 months ago
该专区内容有关ADE电能计量专区的讨论和常见问题解答。 发帖前请阅读 Analog Devices EngineerZone 行为准则。
All Threads
by
Babusuman
ADE电能计量专区
Started
2 months ago
101
0
0
Not Answered
Regarding Power Factor and Power Measurement Accuracy Using CT on CT Secondary with ADE7880
0
Not Answered
Dear All, Thanks for all your support. we currently developing a three-phase power quality monitoring device based on the ADE7880 energy metering IC. The system measures voltage, current, power factor, active power, reactive power, and harmonic...
Analog to Digital Converters (ADCs)
hardware
101
0
0
by
TPSON
ADE电能计量专区
Started
3 months ago
103
0
0
Not Answered
ADE7858 无法输出CF
0
Not Answered
SPIWrite2Bytes(Gain,0x0000); //电流增益/电压增益都设置成1,config the Gain of the PGA , which is before the ADC of ADE7878 rturnvalue = SPIRead2Bytes(Gain); if(rturnvalue == 0) { rturnvalue = 1; } SPIWrite2Bytes(CONFIG,0x0000); //默认 SPIWrite2Bytes(HPFDIS,0x0000);...
Energy Metering ICs
Integrated/Special Purpose A/D Converters
103
0
0
by
JimHuang
ADE电能计量专区
Started
5 months ago
162
0
0
Not Answered
ADE7913测试ADC输出码的标称值差异较大
0
Not Answered
DE7913测试发现标称值差异比较大,比如 500mV 下规格书写的是 5320000 ,但我们读取到的可能是 4500000 ,而且每一块 ADE7913 的值差异也比较大,目前不校准的情况下感觉基本就不能用,这个正常吗?谢谢!
162
0
0
by
csppm
ADE电能计量专区
Latest
6 months ago
by
csppm
284
1
0
Not Answered
LTC2959IDDB#TRPBF芯片电流误差为10%
0
Not Answered
我们测试贵公司的LTC2959IDDB#TRPBF芯片时,发现通过芯片所给的mAh算出来的电流和源表所给的电流相差10%,这是为什么呢,这款芯片理论误差不是1%吗
电能累计
计量芯片
battery management
电池管理芯片
284
1
0
by
bit131
ADE电能计量专区
Latest
6 months ago
by
bit131
479
1
0
Not Answered
AD9525配置问题
0
Not Answered
AD9528根据官网进行配置成当前项目所需的,配置始终读取0x508=E8 以下是是依次写入到寄存器,和上位机图,
Clock Generation Devices
Clock Generation and Distribution
hardware
ad9528
479
1
0
by
role99
ADE电能计量专区
Started
7 months ago
186
0
0
Not Answered
ADE7858最多可以测量多少次谐波
0
Not Answered
ADE7858最多可以测量多少次谐波,在硬件设计需要注意哪些地方,谢谢 ADE7880有写最大测量63次谐波,ADE7858手册里面没有找到相关的描述
hardware
ade7858
Energy Metering ICs
Integrated/Special Purpose A/D Converters
186
0
0
by
alexshan
ADE电能计量专区
Latest
7 months ago
by
alexshan
633
3
0
Answered
ADE7880 使用单相问题
0
Answered
AD7880 读不到正确数据, 电压采样电路图如图所示va,vb,vc,vn通过分压电阻然后UAP,UBP,UCP,UN接入7880的对应电压采样引脚, 电流采样如图2所示 现在ADE7880 PM设智PM0工作模式,且往DSP寄存器写入1启动,,然后延时500ms,能够读到checksum寄存器为 0xAFFA63B9说明spi接口可用,然后UA接入开关电源火线,UN接入开关电源零线,其他UB UC管脚悬空,电流检查管脚悬空,读status1寄存器未能读到过零信号,读vrmsa,vrmsb...
Single Channel A/D Converters
Energy Metering ICs
Integrated/Special Purpose A/D Converters
Precision A/D Converters
633
3
0
by
WILLIAMTAKEZO
ADE电能计量专区
Started
over 1 year ago
259
0
0
Not Answered
ds2782方案的电池怎么校准空载电流为0
0
Not Answered
各位专家好,我有个电池使用的是2782的方案,电池在无负载情况下通过 DS2782 EVkit软件读取电池信息后发现有一个1.25mA的电流,想请问一下怎么将这个电流校准为0?
259
0
0
by
rongzhixiong
ADE电能计量专区
Started
over 1 year ago
245
0
0
Not Answered
MAX17211+T 充,放量SOC精度问题
0
Not Answered
最近客户指定的一个这个型号电量计,美信的是充,放电的显示的SOC精度,是如保测试的,请指导!谢谢
245
0
0
by
cldsq
ADE电能计量专区
Latest
over 1 year ago
by
cldsq
552
2
1
Not Answered
ade7880获取不同相位的电压和电压之间的相角,以及不同相位的电流和电流之间的相角,只有ANGLE0有数值,ANGLE1和ANGLE2数值都为0,相电流之间也是这样。急盼专家的解答
0
Not Answered
大侠,你好, 尝试读取寄存器0xE601/0xE602/0xE603(即ANGLE0/ANGLE1/ANGLE2)的时候,发现这三个寄存器的值,总是为0。 不知道原因。请解,谢谢。 【我的情况】我期望得到不同相位的电压和电压之间的相角,以及 不同相位的电流和电流之间的相角, 看到中文版ade7880的p32页, ,COMPMODE的bit10:bit9=01,测量不同相位的电压和电压之间的延迟。 COMPMODE的bit10:bit9=10 ,测量相电流之间的角度。 。 请问为什么我读取相电压之间的值...
552
2
1
View All Threads
by
alexshan
ADE电能计量专区
Latest
7 months ago
by
alexshan
633
3
0
Answered
ADE7880 使用单相问题
0
Answered
AD7880 读不到正确数据, 电压采样电路图如图所示va,vb,vc,vn通过分压电阻然后UAP,UBP,UCP,UN接入7880的对应电压采样引脚, 电流采样如图2所示 现在ADE7880 PM设智PM0工作模式,且往DSP寄存器写入1启动,,然后延时500ms,能够读到checksum寄存器为 0xAFFA63B9说明spi接口可用,然后UA接入开关电源火线,UN接入开关电源零线,其他UB UC管脚悬空,电流检查管脚悬空,读status1寄存器未能读到过零信号,读vrmsa,vrmsb...
Single Channel A/D Converters
Energy Metering ICs
Integrated/Special Purpose A/D Converters
Precision A/D Converters
633
3
0
by
CharlieCJH
ADE电能计量专区
Latest
over 1 year ago
by
CharlieCJH
2294
15
0
Answered
ADE7953 相关问题- 虚功率、ANGLE 输出值 以及如何调整 Offset
0
Answered
1. 设定虚功率时,虚要注意什么吗? 因为在高功率电阻量测时所设定的参数,当量测家电时,数值就不准确了 2. ANGLE 的数值,根据文件所示,是表示电压输入以及电流输入之间的延迟时间,那这样输出直接是相位角了吗? 还是需要经过公式呢 (38 式? 3. 那如何调整 offset 的部分呢? 因为理论来说功率因素与电压电流有关,但我调整电压电流相关的参数,但都只能个别调整,是否他们的通道都是独立的呢? 感谢,希望可以获得答案,辛苦了!
ade7953
Energy Metering ICs
Integrated/Special Purpose A/D Converters
2294
15
0
by
CharlieCJH
ADE电能计量专区
Latest
over 1 year ago
by
YYU3
1004
3
0
Answered
ADE7953 低通滤波器相关问题
0
Answered
若我没有理解错误,目前看文件所示,电压以及电流通道都会经过类比低通滤波器(电路实现),然后再进入Σ-Δ调制器,再进入数位的低通滤波器,那这边的数位低通滤波器是否有记忆体位置存在呢? 想确认是否正确的工作,或者他是一定会工作的? 想要有一个检测的方法,不知道是否有。 再麻烦回答了,大大感谢!
Energy Metering ICs
Integrated/Special Purpose A/D Converters
1004
3
0
by
ABCQSW
ADE电能计量专区
Latest
over 2 years ago
by
YYU3
948
1
0
Answered
MAX17205电量计如何正确配置所有寄存器
0
Answered
第一个问题:MAX17205 用EZ配置电池相关参数,但我发现Empty Voltage最低只能设置为3V,我想设置成2.5V或2.4V有办法实现吗? 第二个问题:我看MAX17205芯片手册,有好多寄存器,许多寄存器都不理解什么意思,我该如何配置它们?哪些寄存器是必须配置的,哪些可以使用默认参数?
hardware
948
1
0
by
cttmoshen
ADE电能计量专区
Latest
over 2 years ago
by
YYU3
705
1
0
Answered
AD5293BRUZ-100 Vlogic漏电
0
Answered
当我使用 AD5293BRUZ-100时,发现RESET AD5293BRUZ-100后,会有2.0V电压从Vlogic漏电到我的电源上,导致我的MCU继续工作
hardware
AD5293BRUZ-100
705
1
0
by
kevinxiao
ADE电能计量专区
Latest
over 2 years ago
by
YYU3
797
1
0
Answered
Enable "Multipoint Phase/Gain Calibration" fail, why?
0
Answered
I try to set MTEN bit in config0 register for ADE9430, when system initialization. but I can see any different Irms with MTEN=0, It seems the MTEN is invalid. The code see below: config = 0; AFEWrite16BitReg(REG_RUN, (uint16_t *)&config); ...
Energy Metering ICs
Integrated/Special Purpose A/D Converters
ADE9430
电能计量
797
1
0
by
TomLiu
ADE电能计量专区
Latest
over 3 years ago
by
Admin_ADI
900
1
0
Answered
ADE9153A的autocalibration功能有没有一些测试数据或性能比较吗?
0
Answered
Dear, 请问ADE9153A的autocalibration功能有没有一些测试数据或性能比较吗?非常感谢!!
900
1
0
by
ABCQSW
ADE电能计量专区
Latest
over 3 years ago
by
Admin_ADI
1215
1
1
Answered
DS2788K的MEMORY TAB什么意思,需要怎么配置?
0
Answered
What does the MEMORY TAB of DS2788K mean and how to configure it?
DS2788K
1215
1
1
by
alexburtakov
ADE电能计量专区
Latest
over 3 years ago
by
AbhishekP
1294
2
0
Answered
LTC6811-1
0
Answered
Hello to ADI support team , I have some questions according LTC6811-1 . I use cascade connection of two LTC6811 for 20S cells connection . 1. I have mode in with Controller is disconnected and both LTC6811-1 operating without external Controller...
battery management
ltc6811-1
Multicell Battery Stack Monitor
1294
2
0
by
JJLIN
ADE电能计量专区
Latest
over 3 years ago
by
Admin_ADI
1254
1
0
Answered
ADE7878A 相位角度讀取問題
0
Answered
大家好 近期開發ADE7878A用來量測電能消耗 但讀取相位角度發生問題,讀取A相的角度有回應值,但讀取B相角度與C相角度的回應值皆為0 能否幫我解惑哪裡設定有錯誤,謝謝。 程式init流程 ( 只會在開機時執行一次 ) Config2(0xEC01) W 0x02 PGA Gain(0xE60F) W 0x00 0x00 AIGAIN(0x4380) W 0x00 0x00 0x00 0x00 AVGAIN(0x4381) W 0x00 0x00 0x00 0x00...
Angle1
Angle2
Energy Metering ICs
Integrated/Special Purpose A/D Converters
ade7878a
Show More
1254
1
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More