多个DS18B20单总线并联,无法正常读取内置ROM的ID
问答
讨论
文档
成员
标签
Cancel
文档
DS18B20+: FAQ
+
DS18B20+PAR: FAQ
-
DS18B20/GG8: FAQ
DS18B20 在现场使用时出现温度在85度和21度之间来回跳变,21度是正常的,通讯距离10米,该如何解决?
DS18B20 正常通信,但是读取转换结果要么是85度要么是128度左右,是什么问题?
DS18B20传感器符合ISO 22000标准吗?
DS18B20可浸在水中吗?
DS18B20和DS2438是否能够挂接在同一1-wire总线上?
DS18B20在0°C至85°C范围下精度指标为±0.5°C,但数据资料的典型曲线仅给出了0°C至70°C范围测试结果。超过该范围后,DS18B20的典型误差曲线如何?
DS18B20总线上各节点的采样时间是否相同?
DS18B20正在转换温度时能发送命令吗?
DS18B20正在转换温度期间,能发送命令吗?
DS18B20测温传感器位于器件的哪个物理位置?
DS18B20的校准有效时间是多长?DS18B20可重新校准吗?
DS18B20的潮湿敏感度等级是多少?
DS18B20的环境特性如何?
DS18B20芯片之间的温度一致性如何?
Maxim是否提供适用于DS18B20的例程或用于相关操作系统的驱动?
什么情况下不推荐DS18B20使用寄生供电?
什么是硅温度传感器?
使用OneWireViewer能够记录多片DS18B20吗?
使用OneWireViewer能够记录多片DS18B20数据吗?
在密封保护DS18B20的外壳时,是否有推荐的黏合剂?
多个DS18B20单总线并联,无法正常读取内置ROM的ID
如何使用多片DS18B20,以及如何知道其1-wire链中的位置?
如何使用示波器抓取远端1-Wire设备信号?
如果我希望将DS18B20与工作在3.3V的微控制器配合使用,那么需要电平转换器吗?
如果我希望将DS18B20与工作在3.3V的微控制器配合使用,需要电平转换器吗?
如果我希望连接1-Wire器件,如何保护微控制器的GPIO端口?
如果我希望连接DS18B20等1-Wire器件,如何保护微控制器的GPIO端口?
对于5V和3.3V供电,DS18B20需要上拉电阻吗?
序列号在所有1-Wire器件中唯一,还是仅在特定DS18B20 1-Wire芯片系列中唯一?
序列号在所有1-Wire器件中唯一,还是仅在特定系列中唯一?同一卷IC的序列号会重复吗?
强磁场是否影响DS18B20的性能?
是否可以通过读取DS18B20的寄存器来检查电源故障?
是否对DS18B20进行过振动试验?
是否提供DS18B20的VHDL或Verilog代码?
是否有办法同时向多个1-wire器件发送相同命令?
是否有办法扩展DS18B20的温度量程?
用处理器实现两个通道读取DS18B20的温度,一个通道能够读取,另一个通道不能够读取,用示波器观察发现不能读取的通道在发送0xCC指令时的波形不对,请问是什么原因导致的?该如何解决?
能利用3V电池为DS18B20供电吗?
能否提供DS18B20接线图和颜色标识?
防潮绝缘涂层是否影响DS18B20的温度响应?
DS18B20/T&R-W: FAQ
+
DS18S20+: FAQ
+
DS2401: FAQ
+
DS2431+: FAQ
DS2431P+T&R: FAQ
+
DS2480B+: FAQ
+
DS2480B: FAQ
+
DS2482-100: FAQ
DS2484: FAQ
+
DS2484Q+T: FAQ
+
DS2488Q+: FAQ
+
DS24B33Q+U: FAQ
+
DS2502+: FAQ
+
DS2502-E48: FAQ
DS2502: FAQ
DS2502P+T&R: FAQ
+
DS2505+: FAQ
+
DS28C36AQ+T: FAQ
+
DS28E01-100+: FAQ
DS28E05: FAQ
+
DS28E05P+: FAQ
+
DS28E07+: FAQ
DS28E07: FAQ
+
DS28E15: FAQ
DS28E17: FAQ
+
DS28E17Q+T: FAQ
+
DS28E38G+T: FAQ
+
DS28E38Q+T: FAQ
+
MAX31820MCR+: FAQ
MAX31850: FAQ
+
MAX31850EATB+: FAQ
+
MAX31850KATB+: FAQ
+
MAX66300-24XEVKIT#: FAQ
在2015年购买的DS2431P+读取内部的存储器数据全部为0x00,但最近购买的一批内部数据不是0x00,是不是Maxim更改了初始值?
在一根电缆上带有11个DS18B20,长度为80米,利用AN244推荐的电路设计1-Wire主机,第一次能够正常读取,以后就会出现温度异常,请问如何解决?
嵌入式安全与1-Wire 标签
我们有一批DS2502编程写错了,请问还可以修改过来吗?有什么办法能够使这些产品继续使用?
通用产品DS2431P+T的地址为0086H和0087H的寄存器的内容为制造商ID,那么这两个寄存器的初始值是什么
多个DS18B20单总线并联,无法正常读取内置ROM的ID
Revision
Creation Date
Revision Author
Select All
Current Revision
19 Dec 2023 6:47 PM
MSDAPI
1
Revision #1
3 Dec 2020 7:01 AM
MSDAPI
Compare Versions
View current version