文档 使用DS2480b芯片时,按照写流程写数据,当写0xe3数据时,识别为了“Set Command Mode”命令,使其0xe3数据无法写入到芯片内,是芯片的bug吗?
  • 问答
  • 文档
  • 成员
  • 标签
  • Cancel
  • 文档
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20/T&R-W: FAQ
  • +DS18S20+: FAQ
  • +DS2401: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • +DS2480B+: FAQ
  • -DS2480B: FAQ
    • DS2480B上电后需要多久MCU才可以通过UART接口和DS2480B进行通讯?
    • DS2480B如何驱动多个DS18B20或1-wire 器件,同时进行温度转换或大电流操作时有什么方案?
    • DS2480B的POL引脚在设置后多久生效?
    • DS2480B编程脉冲时间默认长度不够,如何调节脉冲时间?
    • 使用DS2480b芯片时,按照写流程写数据,当写0xe3数据时,识别为了“Set Command Mode”命令,使其0xe3数据无法写入到芯片内,是芯片的bug吗?
    • 如果DS2480B上电后接收到一个非预期的命令(比如F0),是否会导致DS2480B进入一个不确定状态后挂起?
    • 如果是两个DS2480B的one wire引脚连一起,串口分别接不同设备,是否可以有一个设备作为one wire的从设备使用呢?
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484Q+T: FAQ
  • +DS2488Q+: FAQ
  • +DS24B33Q+U: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28E01-100+: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E07+: FAQ
  • DS28E07: FAQ
  • +DS28E15: FAQ
  • DS28E17: FAQ
  • +DS28E17Q+T: FAQ
  • +DS28E38G+T: FAQ
  • +DS28E38Q+T: FAQ
  • +MAX31820MCR+: FAQ
  • MAX31850: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • 在2015年购买的DS2431P+读取内部的存储器数据全部为0x00,但最近购买的一批内部数据不是0x00,是不是Maxim更改了初始值?
  • 在一根电缆上带有11个DS18B20,长度为80米,利用AN244推荐的电路设计1-Wire主机,第一次能够正常读取,以后就会出现温度异常,请问如何解决?
  • 嵌入式安全与1-Wire 标签
  • 我们有一批DS2502编程写错了,请问还可以修改过来吗?有什么办法能够使这些产品继续使用?
  • 通用产品DS2431P+T的地址为0086H和0087H的寄存器的内容为制造商ID,那么这两个寄存器的初始值是什么

使用DS2480b芯片时,按照写流程写数据,当写0xe3数据时,识别为了“Set Command Mode”命令,使其0xe3数据无法写入到芯片内,是芯片的bug吗?

 

这种情况的确存在,对于这种情况的处理是: 如果发送的数据和切换到命令模式的命令(E3)相同时,要重复发送这个字节,这样就是告诉DS2480B要将0xE3作为数据处理而不是切换模式,下面的示例程序供您参考:

int OWBlock(unsigned char *tran_buf, int tran_len)
{
   unsigned char sendpacket[320];
   unsigned char sendlen=0,pos,i;

   // check for a block too big
   if (tran_len > 160)
      return FALSE;

   // construct the packet to send to the DS2480B
   // check for correct mode
   if (UMode != MODSEL_DATA)
   {
      UMode = MODSEL_DATA;
      sendpacket[sendlen++] = MODE_DATA;
   }

   // add the bytes to send
   pos = sendlen;
   for (i = 0; i < tran_len; i++)
   {
      sendpacket[sendlen++] = tran_buf[i];

      // duplicate data that looks like COMMAND mode
      if (tran_buf[i] == MODE_COMMAND)
         sendpacket[sendlen++] = tran_buf[i];             //重复发送和命令相同的字节

   }

   // flush the buffers
   FlushCOM();

   // send the packet
   if (WriteCOM(sendlen,sendpacket))
   {
      // read back the response
      if (ReadCOM(tran_len,tran_buf) == tran_len)
         return TRUE;
   }

   // an error occured so re-sync with DS2480B
   DS2480B_Detect();

   return FALSE;
}
 

 

Tags: DS2480B 嵌入式安全与1-Wire KA-01690