文档 我们有一批DS2502编程写错了,请问还可以修改过来吗?有什么办法能够使这些产品继续使用?
  • 问答
  • 文档
  • 成员
  • 标签
  • Cancel
  • 文档
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20/T&R-W: FAQ
  • +DS18S20+: FAQ
  • +DS2401: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • +DS2480B+: FAQ
  • +DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484Q+T: FAQ
  • +DS2488Q+: FAQ
  • +DS24B33Q+U: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28E01-100+: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E07+: FAQ
  • DS28E07: FAQ
  • +DS28E15: FAQ
  • DS28E17: FAQ
  • +DS28E17Q+T: FAQ
  • +DS28E38G+T: FAQ
  • +DS28E38Q+T: FAQ
  • +MAX31820MCR+: FAQ
  • MAX31850: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • 在2015年购买的DS2431P+读取内部的存储器数据全部为0x00,但最近购买的一批内部数据不是0x00,是不是Maxim更改了初始值?
  • 在一根电缆上带有11个DS18B20,长度为80米,利用AN244推荐的电路设计1-Wire主机,第一次能够正常读取,以后就会出现温度异常,请问如何解决?
  • 嵌入式安全与1-Wire 标签
  • 我们有一批DS2502编程写错了,请问还可以修改过来吗?有什么办法能够使这些产品继续使用?
  • 通用产品DS2431P+T的地址为0086H和0087H的寄存器的内容为制造商ID,那么这两个寄存器的初始值是什么

我们有一批DS2502编程写错了,请问还可以修改过来吗?有什么办法能够使这些产品继续使用?

DS2502是EPROM,该器件只能将内部寄存器的1改成0,而不能将0改回1,因此,通常将DS2502当作一次性可编程产品。如果您想继续使用该产品,可以利用器件内部的重定向功能,关于如何使用该功能,请参考数据手册中的“EPROM STATUS BYTES”中关于重定向页面的描述。
Tags: 000097610 DS2502P+T&R
  • Share
  • History
  • Cancel
 
Related Content
  • DS2502P+T&R: FAQ
    MSDAPI
    DS2502P+T&R: FAQ
  • DS2502P+T&R: FAQ
    MSDAPI
    DS2502P+T&R: FAQ
  • RE: flash driver
    ADIApproved
    Hi, As you might already know, ADSP-21061 EZ-Kit doesn't have a FLASH but has an EPROM. EPROM can't be programmed using the DSP and therefore there is no driver file available for the same. One way to...
 
Related Content
  • DS2502P+T&R: FAQ
    MSDAPI
    DS2502P+T&R: FAQ
  • DS2502P+T&R: FAQ
    MSDAPI
    DS2502P+T&R: FAQ
  • RE: flash driver
    ADIApproved
    Hi, As you might already know, ADSP-21061 EZ-Kit doesn't have a FLASH but has an EPROM. EPROM can't be programmed using the DSP and therefore there is no driver file available for the same. One way to...