Post Go back to editing

有哪些UART或RS-232转1-Wire的接口器件?

有哪些UARTRS-2321-Wire的接口器件?

  • DS2480B。该器件可以将主机的RS-232信号(需要反相器)或者直接将UART信号转换为1-Wire信号,从而实现了利用一对串口(TX和RX)控制多个从机的功能。由于DS2480B内部带有定时器,因此主机就不需要额外生成满足1-Wire协议的严格时序。需要指出的是,DS2480B仅仅支持±5V的RS-232电平,如果RS-232电平为±12V,则需要额外的钳位电路和电平转换器。此外,DS2480B还可以设置四种不同的通信速率,包括115.2kbps、57.6kbps、19.2kbps和9.6kbps,默认速率为9.6kbps。