Members
Tags
Cancel
文档
MAX
MAX31850KATB+: FAQ
More
Cancel
MAX31850存储器中"Cold-Junction-Compensated (Byte0、Byte1)"存放的是补偿后的热端温度值吗?是否可以直接使用,是否还需要做其它补偿?
Byte0和Byte1中存放的数据是经过冷端补偿后的热电偶温度数据,可以直接使用。由于热电偶的输出电压和温度之间呈现非线性关系,但是MAX31850在进行温度转换时把热电偶的输出电压和温度之间的关系当作线性来处理,当热电偶温度增大或者减小时,这种非线性使得MAX31850测量到的温度误差增大。通常在-25ºC至160ºC温度范围内误差为1ºC,如果测量的温度范围更宽,误差随之增大,可以根据设计的需要进行修正
在测试MAX31850时,当对热电偶加热,由于PCB离热源较近,导致温度误差增大,应该如何进行修正才能得到正确的温度?
由于热电偶测温需要冷端补偿,MAX31850采用内部温度传感器作为温度补偿,如果在使用中热电偶的实际冷端与MAX31850器件之间有温度差,这样就会造成测温误差,由于这个温度差未知,因此无法进行补偿,为确保正确测温,需要保证热电偶冷端和MAX31850温度一致。 另外热电偶本身测量是非线性的,但是MAX31850器件内部把热电偶转换当成了线性进行处理,因此,在测量较高温度或者较低温度时误差会比较大…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.