DS2502+: FAQ
文档
问答
Members
Tags
Cancel
文档
DS2x
DS2502+: FAQ
Created
over 8 years ago
Updated
3 months ago
Was this helpful?
Yes
No
More
Cancel
DS2502EVKIT Li+电池电压范围及如何搭建PC通信?
VDD和VSS之间电压的推荐范围为2.8V至6V @ - 40°C至+85°C。可利用电源代替电池连接。DS2502评估板通过DS9123O USB适配器和RJ-11电缆连接到PC。用户通过标准6芯RJ-11线连接,与DS2502通信。
DS2502全球唯一的48位节点地址是否就是设备连网用的MAC地址?
DS2502有多个版本,带有MAC地址的版本是DS2502P-E48+,这是TSOC-6封装的,其他的版本不带有MAC地址。请确认您购买的产品型号是否正确。
如何将数据写入DS2502?
关于DS2502写EPROM的问题,过程如下: 1. 发送复位脉冲,检测DS2502应答信号。 2.发送SKIPROM命令或者其他ROM命令。 3.发送Write Memory命令0x0F. 4.发送要写的寄存器地址:低字节,高字节 5.发送要写入该地址的数据。 6.主机读取CRC验证写入数据是否正确? 如果不正确,回到第1步。 7.此时,将1-Wire总线上拉到12V编程电压,等待数据写入寄存器…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.