DS2484Q+T: FAQ

  • Created
  • Updated
Was this helpful?
  • 1-Wire总线过压和过流保护

    对于过压保护,考虑使用串联2个5Ω电阻的5.6V齐纳二极管(每端一个)。两个5Ω电阻的目的是防止1-Wire总线上的电压超过5.6V,相对于导通二极管呈高阻。这就造成在DS2484的另一侧与电路产生一定的隔离。 如果同时需要过压和过流保护,推荐具有高精度的MAX14588可调节保护器。可调节过压范围,最高36V,过压范围可低至6V (适合于DS2484 IO引脚的最大电压指标)。此外,限流保护可低至15mA…
  • 在设计应用中需要两个DS2484主机来驱动一个1-Wire 总线,如果一个DS2484主机掉电,另外一个DS2484是否可以工作?

    对于1-Wire总线的驱动是可以支持多主机的工作方式,但是在任意时刻只能有一个1-Wire主机驱动总线,当主机驱动总线为高电平时,如果另一个主机掉电,器件内部的保护二极管会导通,这样就会把总线拉低,导致无法正常工作。
  • 有没有可以实现远距离的IIC通讯解决方案?

    可以选择DS2484和DS28E18配合使用,DS2484是IIC到1-Wire桥接器,1-Wire总线可以支持远距离通讯,DS28E18是1-Wire到IIC主机转换器。DS2484和处理器在一端, DS28E18和被控制的IIC器件在远端,它们之间利用单总线连接。这种转换需要对DS2484和DS28E18进行编程,另外,1-Wire通讯速率不是太高。但是可以实现IIC的远距离通讯。
  • 调试DS2484和DS18B20通讯,在对DS18B20单独供电时,工作正常;采用寄生供电时,无法启动转换,读取的结果是上电默认值,是什么原因?

    当DS18B20采用寄生供电时,要将DS18B20的电源引脚和GND连接到一起,不要将DS18B20 VDD引脚悬空。当发送完温度转换命令后,在电源供电条件下由外部电源提供供电,对总线的要求不高,但是在寄生供电条件下,需要总线来提供电源,因此在温度转换期间(通常为750ms)要保证总线一直为高电平且总线电压不能低于3V,因此,在总线供电的应用中,在温度转换期间通常需要启动DS2484的强上拉,而且供电电源要选择5V…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.