There are no internal pull-up/pull-down resistors on the Address pins of the DS1744. These pins can be tied directly to VCC or GND to set a fixed logic state.
DS1744P
Production
The DS1744 is a full-function, year-2000-compliant (Y2KC), real-time clock/calendar (RTC) and 32k x 8 NV SRAM. User access to all registers within the...
Datasheet
DS1744P on Analog.com
There are no internal pull-up/pull-down resistors on the Address pins of the DS1744. These pins can be tied directly to VCC or GND to set a fixed logic state.