Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Clocks & Timers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Clocks & Timers
Clocks & Timers
Documents Do RTC VCC falling rate affect the back-up battery feature?
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel

Products Mentioned

DS1340C Production
The DS1340 is a real-time clock (RTC)/calendar that is pin compatible and functionally equivalent to the ST M41T00, including the software clock calibration...
Datasheet
DS1340C on Analog.com

DS1302 Production
The DS1302 trickle-charge timekeeping chip contains a real-time clock/calendar and 31 bytes of static RAM. It communicates with a microprocessor via a...
Datasheet
DS1302 on Analog.com

Associated Drivers

Table of Contents
  • +Documents
  • Clock and Timing Support Community
  • +AD9508: FAQ
  • +AD9510: FAQ
  • +AD9511: FAQ
  • +AD9512: FAQ
  • +AD9513: FAQ
  • +AD9514: FAQ
  • +AD9515: FAQ
  • +AD9517-1: FAQ
  • +AD9518-0: FAQ
  • +AD9518-4: FAQ
  • +AD951x: FAQ
  • +AD9520-3: FAQ
  • +AD9523-1: FAQ
  • +AD9523: FAQ
  • +AD9525: FAQ
  • +AD9548: FAQ
  • +AD9549BCPZ: FAQ
  • +AD9552: FAQ
  • AD9951: FAQ
  • AD9957: FAQ
  • +ADCLK846: FAQ
  • +LTC6952: FAQ
  • +LTC695x: FAQ
  • +AD2S99: FAQ
  • +AD9518-3: FAQ
  • +AD9523-1/PCBZ: FAQ
  • +AD9558: FAQ
  • +AD9560: FAQ
  • +AD9577: FAQ
  • +ADCLK925: FAQ
  • +ADN2812: FAQ
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • +ADN2817: FAQ
  • Can you share the thermal data of DS1672U-33+T&R?
  • Does reset output of DS3232 affect internal RTC counting?
  • +DS1023-50: FAQ
  • DS1023: FAQ
  • +DS1023S-100+: FAQ
  • +DS1050U-001: FAQ
  • +DS1080LU+: FAQ
  • +DS1086LU+: FAQ
  • +DS1090: FAQ
  • +DS1091LUA-330+T: FAQ
  • +DS1099: FAQ
  • +DS1110S-50+: FAQ
  • +DS1124U-25+: FAQ
  • +DS1244W-120+: FAQ
  • +DS1251W-120IND+: FAQ
  • +DS12887+: FAQ
  • DS12887: FAQ
  • +DS12C887+: FAQ
  • +DS12C887A+: FAQ
  • +DS12CR887-33+: FAQ
  • -DS1302+: FAQ
    • Do RTC VCC falling rate affect the back-up battery feature?
    • Does the DS1302 have internal diodes and resistors for the trickle charger, or do I need to add them externally?
    • In what circumstances would the CH bit of the seconds register in the DS1302 automatically set to 1?
    • Is there any prbolem if the VCC1 and VCC2 pins of DS1302 are reverse connected?
    • We ordered some DS1302ZN. However, the N was not printed right after the part number on the top mark of the chip. Did we order the wrong model number? Or was there a new version from the factory?
    • What's the key error for a crystal?
  • DS1302: FAQ
  • +DS1306+: FAQ
  • +DS1307+: FAQ
  • DS1307: FAQ
  • +DS1315-33+: FAQ
  • +DS1337: FAQ
  • +DS1338U-33+: FAQ
  • DS1339A: FAQ
  • +DS1339AU+: FAQ
  • +DS1339C-33#: FAQ
  • +DS1339U-3+: FAQ
  • +DS1340U-3+: FAQ
  • +DS1341: FAQ
  • +DS1342T+: FAQ
  • +DS1343D-18+: FAQ
  • +DS1347T+: FAQ
  • +DS1374: FAQ
  • +DS1375T+: FAQ
  • +DS1388Z-3+: FAQ
  • +DS1388Z-33: FAQ
  • +DS1390U-18+: FAQ
  • +DS1390U-33/V+T: FAQ
  • +DS1501: FAQ
  • +DS1554-70IND+: FAQ
  • DS1672U-33+T&R: FAQ
  • +DS1682: FAQ
  • +DS1682S+: FAQ
  • DS1683: FAQ
  • +DS1683S+: FAQ
  • +DS1687-3+: FAQ
  • +DS1687-3IND: FAQ
  • +DS1744W-120+: FAQ
  • +DS1744W-120IND+: FAQ
  • +DS1744WP-120+: FAQ
  • +DS1746W-120+: FAQ
  • +DS1747-70IND+: FAQ
  • +DS26503L+: FAQ
  • DS3231: FAQ
  • +DS3231M+: FAQ
  • DS3231M: FAQ
  • +DS3231MPMB1#: FAQ
  • +DS3231MZ/V+: FAQ
  • +DS3231S#: FAQ
  • +DS3231SN#T&R: FAQ
  • DS3232M: FAQ
  • +DS3232MZ+: FAQ
  • DS3232SN#T&R: FAQ
  • +DS3234S#: FAQ
  • +DS3234SN#: FAQ
  • +DS32KHZ/WBGA+: FAQ
  • +DS32KHZN/WBGA: FAQ
  • +HMC-T2220: FAQ
  • +HMC704X and HMC704XB: FAQ
  • +ICM7217: FAQ
  • +ICM7240C/D: FAQ
  • +LTC1799: FAQ
  • +MAX31329: FAQ
  • +MAX31331: FAQ
  • MAX31341BEWC+: FAQ
  • +MAX31341BEWC+T: FAQ
  • +MAX31343EKA+: FAQ
  • +MAX3841: FAQ
  • +MAX3872AETJ+: FAQ
  • +MAX9180EXT+: FAQ
  • +MAX9394EHJ+: FAQ
  • What is the FIT rate of the DS3231SN#T&R for different temperatures?

Do RTC VCC falling rate affect the back-up battery feature?

Maxim's RTC like DS1302,DS1399,DS1340 have back-up battery feature , allowing RTC to continue work during VCC fail time. But sometime customer find after VCC fail and recover, they can not read RTC time correctly. This is possible caused by the falling rate of VCC. VCC falls under lowest supply voltage before the internal power rail switches to Vbat.

These parts requires the falling rate of VCC being 0.27V/300us. (3.3V VCC)For 3V and 1.8V VCC, please refer to table below.

So to avoid power down between switching from VCC to Vbat, enough capacitor should be added at the VCC pin.

 

Tags: DS1302+ Serial Address RTCs KA-02697 RTC ,Back-up battery,DS1302,DS1339 Real-Time Clocks DS1340 ds1302 Show More