Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Clocks & Timers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Clocks & Timers
Clocks & Timers
Documents AD9523-1 interfacing with HMC832, DAC/ADC- input and output considerations
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel

Products Mentioned

HMC832A Last Time Buy
The HMC832A is a 3.3 V, high performance, wideband, fractional-N, phase-locked loop (PLL) that features an integrated voltage controlled oscillator (VCO...
Datasheet
HMC832A on Analog.com

HMC8325 Recommended for New Designs
The HMC8325 is an integrated E-band gallium arsenide (GaAs), monolithic microwave integrated circuit (MMIC), low noise amplifier (LNA) chip that operates...
Datasheet
HMC8325 on Analog.com

AD9523 Not Recommended for New Designs
The AD9523 provides a low power, multi-output, clock distribution function with low jitter performance, along with an on-chip PLL and VCO. The on-chip...
Datasheet
AD9523 on Analog.com

Associated Drivers

AD9523-1 Recommended for New Designs
The AD9523-1 provides a low power, multi-output, clock distribution function with low jitter performance, along with an on-chip PLL and VCO with two VCO...
Datasheet
AD9523-1 on Analog.com

Associated Drivers

HMC8327 Obsolete
The HMC8327LG is a fully integrated System In Package (SiP) in-phase/quadrature (I/Q) downconverter that operates between an RF input frequency range of...
Datasheet
HMC8327 on Analog.com

HMC8326 Obsolete
The HMC8326LG is a fully integrated System In Package (SiP) in-phase/quadrature (I/Q) downconverter that operates between an RF input frequency range of...
Datasheet
HMC8326 on Analog.com

Table of Contents
  • +Documents
  • Clock and Timing Support Community
  • +AD9508: FAQ
  • +AD9510: FAQ
  • +AD9511: FAQ
  • +AD9512: FAQ
  • +AD9513: FAQ
  • +AD9514: FAQ
  • +AD9515: FAQ
  • +AD9517-1: FAQ
  • +AD9518-0: FAQ
  • +AD9518-4: FAQ
  • +AD951x: FAQ
  • +AD9520-3: FAQ
  • -AD9523-1: FAQ
    • AD9523-1 interfacing with HMC832, DAC/ADC- input and output considerations
    • AD9523-1: Can I bypass PLL1 and only use the PLL2?
  • +AD9523: FAQ
  • +AD9525: FAQ
  • +AD9548: FAQ
  • +AD9549BCPZ: FAQ
  • +AD9552: FAQ
  • AD9951: FAQ
  • AD9957: FAQ
  • +ADCLK846: FAQ
  • +LTC6952: FAQ
  • +LTC695x: FAQ
  • +AD2S99: FAQ
  • +AD9518-3: FAQ
  • +AD9523-1/PCBZ: FAQ
  • +AD9558: FAQ
  • +AD9560: FAQ
  • +AD9577: FAQ
  • +ADCLK925: FAQ
  • +ADN2812: FAQ
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • +ADN2817: FAQ
  • Can you share the thermal data of DS1672U-33+T&R?
  • Does reset output of DS3232 affect internal RTC counting?
  • +DS1023-50: FAQ
  • DS1023: FAQ
  • +DS1023S-100+: FAQ
  • +DS1050U-001: FAQ
  • +DS1080LU+: FAQ
  • +DS1086LU+: FAQ
  • +DS1090: FAQ
  • +DS1091LUA-330+T: FAQ
  • +DS1099: FAQ
  • +DS1110S-50+: FAQ
  • +DS1124U-25+: FAQ
  • +DS1244W-120+: FAQ
  • +DS1251W-120IND+: FAQ
  • +DS12887+: FAQ
  • DS12887: FAQ
  • +DS12C887+: FAQ
  • +DS12C887A+: FAQ
  • +DS12CR887-33+: FAQ
  • +DS1302+: FAQ
  • DS1302: FAQ
  • +DS1306+: FAQ
  • +DS1307+: FAQ
  • DS1307: FAQ
  • +DS1315-33+: FAQ
  • +DS1337: FAQ
  • +DS1338U-33+: FAQ
  • DS1339A: FAQ
  • +DS1339AU+: FAQ
  • +DS1339C-33#: FAQ
  • +DS1339U-3+: FAQ
  • +DS1340U-3+: FAQ
  • +DS1341: FAQ
  • +DS1342T+: FAQ
  • +DS1343D-18+: FAQ
  • +DS1347T+: FAQ
  • +DS1374: FAQ
  • +DS1375T+: FAQ
  • +DS1388Z-3+: FAQ
  • +DS1388Z-33: FAQ
  • +DS1390U-18+: FAQ
  • +DS1390U-33/V+T: FAQ
  • +DS1501: FAQ
  • +DS1554-70IND+: FAQ
  • DS1672U-33+T&R: FAQ
  • +DS1682: FAQ
  • +DS1682S+: FAQ
  • DS1683: FAQ
  • +DS1683S+: FAQ
  • +DS1687-3+: FAQ
  • +DS1687-3IND: FAQ
  • +DS1744W-120+: FAQ
  • +DS1744W-120IND+: FAQ
  • +DS1744WP-120+: FAQ
  • +DS1746W-120+: FAQ
  • +DS1747-70IND+: FAQ
  • +DS26503L+: FAQ
  • DS3231: FAQ
  • +DS3231M+: FAQ
  • DS3231M: FAQ
  • +DS3231MPMB1#: FAQ
  • +DS3231MZ/V+: FAQ
  • +DS3231S#: FAQ
  • +DS3231SN#T&R: FAQ
  • DS3232M: FAQ
  • +DS3232MZ+: FAQ
  • DS3232SN#T&R: FAQ
  • +DS3234S#: FAQ
  • +DS3234SN#: FAQ
  • +DS32KHZ/WBGA+: FAQ
  • +DS32KHZN/WBGA: FAQ
  • +HMC-T2220: FAQ
  • +HMC704X and HMC704XB: FAQ
  • +ICM7217: FAQ
  • +ICM7240C/D: FAQ
  • +LTC1799: FAQ
  • +MAX31329: FAQ
  • +MAX31331: FAQ
  • MAX31341BEWC+: FAQ
  • +MAX31341BEWC+T: FAQ
  • +MAX31343EKA+: FAQ
  • +MAX3841: FAQ
  • +MAX3872AETJ+: FAQ
  • +MAX9180EXT+: FAQ
  • +MAX9394EHJ+: FAQ
  • What is the FIT rate of the DS3231SN#T&R for different temperatures?

AD9523-1 interfacing with HMC832, DAC/ADC- input and output considerations

Question

1. We will plan to feed HMC832 with 50 Mhz REF clock. And our design will include 3 pieces of HMC832. So we don't want to delays between REFClocks. And our design also includes a clock generator/distributor. And clock generator/distributor is able to give LVPECL/LVDS/HSDS output. So weare not able to feed with Sinusoidal wave. There is a option to change clock distributor which is able to give LVCMOS output. So we haveLVPECL/LVDS/HSDS/LVCMOS signal types to feed HMC832.Could you able to say which signal type is suitable for HMC832? LVCMOS parameters match with datasheet values. Are we right?(See the answer for the first part below to understand the second question)
2. We try to find a  jitter cleaner clock  distributor for  our ADC, DAC and PLL+VCO. Firstly clock  distributor have to provide clean up  andaccept sine wave input and LVDS input.  So  can we  apply 10 MHz  LVDS and Sine wave  to AD9523-1's reference input? And  also we  will use HMC832as PLL+VCO. Previously we  asked HMC832 reference input type, LVCMOS was recommended. So Is AD9523-1 LVCMOS suitable for HMC832 reference input?

Answer

1. You are correct. Use a LVCMOS driver with 100? termination resistor at each HMC832. The LVCMOS driver meets the minimum signal level requirementsbut may overdrive the reference input without the 100? termination resistor. We find this scheme works well with our eval boards but in general anydesign that meets the specified levels in Table 8 will work. LVPECL/LVDS/HSDS drivers do not provide the necessary output swing.Figures 34 and 37 in DS show better FOM numbers with 50MHz square wave references. This is due to the fast edge rates compared to a sine wave butthere is a concern. A well terminated and isolated reference transmission line will perform well but the fast edges at higher reference frequenciesmake terminating this line difficult. For example we need a 100? resistor to reduce the signal amplitude on the LVCMOS driver but this does notprovide a perfect match to a 50? transmission line. Extremely fast edge rates with this design will not perform well – especially if thetransmission line is long and/or not isolated from other signals . This is the reason we prefer sine waves for higher frequency references as statedin Table 8.

















2. My understanding based on Q1 and Q2 looks like this-(10MHz LVDS or sine wave to) AD9523-1 è ADC/DAC and (50MHz to) 3x HMC832.·For 10MHz LVDS reference into AD9523-1, yes, it is fine.· For 10MHz sine wave, if sine wave has 0dBm power level into 50ohm load, then the slew rate is only 0.02V/nS, which is too low.· For 10MHz sine wave, if sine wave has 7dBm power level into 50ohm load, then the slew rate is only 0.55V/nS, which is ok.
Extremely low slew rate on AD9523-1 reference input would cause in-band noise increasing. I attached a PDF file to show if input slew rate is low,the impact on output in-band noise. In this case, AD9523-1 first PLL may set to a narrow loop bandwidth (such as 100Hz or so), but its outputperformance is still impacted within the bandwidth. You need to pay attention to this degradation.
Let's look at HMC832's input :









Though it did not specify the common-mode voltage on the input, from the Table8, HMC832 DS on Reference Sensitivity-






















we can see maximum square-wave input swing is 2.5V, which implies at AC-coupling condition, +/-1.25V around the common-mode so that the ESD diodesare not turned on. We can use this information to design the drive signal (from AD9523-1).
An easy way, as we discussed previously is to use LVCMOS output format on AD9523-1 to drive REF-IN on HMC832. The problem is the loading – generallyspeaking, all CMOS drivers are NOT designed to drive heavy loading such as 50 ohms, but to drive capacitive loading, such as 10pF. AD9523-1’s CMOSoutputs are same, and they are NOT designed for heavy loading.
Since AD9523-1’s CMOS output swing is 3.3V which is greater than what HMC832 can handle, we can use a resistor divider to divide down the swing andto increase the load resistance (reduce the loading). For example, we can place the external 100 ohm in series with the signal path (instead of inparallel with the REF input pin to GND on HMC832). This would reduce the swing roughly to 50% of 3.3V, but increase the load resistance to 200 ohmtotal. For 50MHz signal frequency, the HMC832’s input capacitance 5pF should be included in the simulations to determine the total loading forAD9523-1’s CMOS driver. Typically, such REF input likes to see near to maximum large swing on it, so you can adjust the series resistance value toget slightly larger swing than 50% of 3.3V. In any cases we discussed (add 100 ohm series R or slightly reduced series R), the total load resistance(or total load including capacitance) of the CMOS driver should be > 100 ohm (roughly around 150 ohms), which is ok for AD9523-1 (better than 50 ohmsloading).









Another small suggestion is Don’t design 50 ohm PCB trace for CMOS driver, instead, design something with less capacitance (which means something hashigh impedance – small trace width means less capacitance but high impedance). This is because CMOS driver is NOT designed for 50 ohm loading.


Tags: Clock Generation Devices ad9523 Clock Generation and Distribution 6AGW1220 Clocks & Timers Fractional-N PLL ad9523-1 Phase Locked Loop (PLL) Synthesizer & Translation Loop hmc832 Show More