Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

EngineerZone
EngineerZone
Clocks & Timers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Clocks & Timers
Clocks & Timers
Documents AD9511: Programming the device in RESET
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9511 Recommended for New Designs
The AD9511 provides a multi-output clock distribution function along with an on-chip PLL core. The design emphasizes low jitter and phase noise to maximize...
Datasheet
AD9511 on Analog.com

Table of Contents
  • +Documents
  • Clock and Timing Support Community
  • +AD9508: FAQ
  • +AD9510: FAQ
  • -AD9511: FAQ
    • AD9511: Programming the device in RESET
    • Baking the AD9951A
    • Want to use AD9510/11's DLD as our lock alarm, but it may not work properly if the reference disappears. Any solution?
  • +AD9512: FAQ
  • +AD9513: FAQ
  • +AD9514: FAQ
  • +AD9515: FAQ
  • +AD9517-1: FAQ
  • +AD9518-0: FAQ
  • +AD9518-4: FAQ
  • +AD951x: FAQ
  • +AD9520-3: FAQ
  • +AD9523-1: FAQ
  • +AD9523: FAQ
  • +AD9525: FAQ
  • +AD9548: FAQ
  • +AD9549BCPZ: FAQ
  • +AD9552: FAQ
  • AD9951: FAQ
  • AD9957: FAQ
  • +ADCLK846: FAQ
  • +LTC6952: FAQ
  • +LTC695x: FAQ
  • +AD2S99: FAQ
  • +AD9518-3: FAQ
  • +AD9523-1/PCBZ: FAQ
  • +AD9558: FAQ
  • +AD9560: FAQ
  • +AD9577: FAQ
  • +ADCLK925: FAQ
  • +ADN2812: FAQ
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • +ADN2817: FAQ
  • Can you share the thermal data of DS1672U-33+T&R?
  • Does reset output of DS3232 affect internal RTC counting?
  • +DS1023-50: FAQ
  • DS1023: FAQ
  • +DS1023S-100+: FAQ
  • +DS1050U-001: FAQ
  • +DS1080LU+: FAQ
  • +DS1086LU+: FAQ
  • +DS1090: FAQ
  • +DS1091LUA-330+T: FAQ
  • +DS1099: FAQ
  • +DS1110S-50+: FAQ
  • +DS1124U-25+: FAQ
  • +DS1244W-120+: FAQ
  • +DS1251W-120IND+: FAQ
  • +DS12887+: FAQ
  • DS12887: FAQ
  • +DS12C887+: FAQ
  • +DS12C887A+: FAQ
  • +DS12CR887-33+: FAQ
  • +DS1302+: FAQ
  • DS1302: FAQ
  • +DS1306+: FAQ
  • +DS1307+: FAQ
  • DS1307: FAQ
  • +DS1315-33+: FAQ
  • +DS1337: FAQ
  • +DS1338U-33+: FAQ
  • DS1339A: FAQ
  • +DS1339AU+: FAQ
  • +DS1339C-33#: FAQ
  • +DS1339U-3+: FAQ
  • +DS1340U-3+: FAQ
  • +DS1341: FAQ
  • +DS1342T+: FAQ
  • +DS1343D-18+: FAQ
  • +DS1347T+: FAQ
  • +DS1374: FAQ
  • +DS1375T+: FAQ
  • +DS1388Z-3+: FAQ
  • +DS1388Z-33: FAQ
  • +DS1390U-18+: FAQ
  • +DS1390U-33/V+T: FAQ
  • +DS1501: FAQ
  • +DS1554-70IND+: FAQ
  • DS1672U-33+T&R: FAQ
  • +DS1682: FAQ
  • +DS1682S+: FAQ
  • DS1683: FAQ
  • +DS1683S+: FAQ
  • +DS1687-3+: FAQ
  • +DS1687-3IND: FAQ
  • +DS1744W-120+: FAQ
  • +DS1744W-120IND+: FAQ
  • +DS1744WP-120+: FAQ
  • +DS1746W-120+: FAQ
  • +DS1747-70IND+: FAQ
  • +DS26503L+: FAQ
  • DS3231: FAQ
  • +DS3231M+: FAQ
  • DS3231M: FAQ
  • +DS3231MPMB1#: FAQ
  • +DS3231MZ/V+: FAQ
  • +DS3231S#: FAQ
  • +DS3231SN#T&R: FAQ
  • DS3232M: FAQ
  • +DS3232MZ+: FAQ
  • DS3232SN#T&R: FAQ
  • +DS3234S#: FAQ
  • +DS3234SN#: FAQ
  • +DS32KHZ/WBGA+: FAQ
  • +DS32KHZN/WBGA: FAQ
  • +HMC-T2220: FAQ
  • +HMC704X and HMC704XB: FAQ
  • +ICM7217: FAQ
  • +ICM7240C/D: FAQ
  • +LTC1799: FAQ
  • +MAX31329: FAQ
  • +MAX31331: FAQ
  • MAX31341BEWC+: FAQ
  • +MAX31341BEWC+T: FAQ
  • +MAX31343EKA+: FAQ
  • +MAX3841: FAQ
  • +MAX3872AETJ+: FAQ
  • +MAX9180EXT+: FAQ
  • +MAX9394EHJ+: FAQ
  • What is the FIT rate of the DS3231SN#T&R for different temperatures?

AD9511: Programming the device in RESET

Question

While the device is in RESET is it possible to program any register to any
value other than the default ?

Answer

It is not possible to program the AD9511 while it is in RESET state. This is
because the RESETB pin (or the soft-reset bit) initiates a sequence of events,
one of which is to reload the default values into the register map. So, even if
you write new values into registers while holding RESET_B low, the reset
operation which ensues when you release RESETB will load the default values
(hardwired) into the registers - so the attempted programming will be
ineffective.

It is possible, however, to hold the outputs in a fixed (non-toggling)
condition by holding the SYNCB signal low. First set the FUNCTION pin to act as
SYNCB. Then, pull the FUNCTION pin low. All outputs which are not explicitly
masked, or are divide-by-1 (divider bypassed) will stop toggling and assume a
preset state. Upon releasing SYNCB, the outputs which were stopped will resume
toggling, but synchronized according to their presets.

Tags: Clock Generation Devices Clock Generation and Distribution Clocks & Timers ad9511 5GFW5335
  • Share
  • History
  • Cancel
 
Related Content
  • RE: Write EEPROM through ADAU1452
    DaveThib
    Hello Dovydas, It was as I thought might happen. When you trigger the soft reset it is just like toggling the reset pin and so the part selfboots. Since the PLL is already up and locked it seems to happen...
  • RE: Question about AD9910 "resetb" bit of CFR3..
    ADIApproved
    1) The "b" in resetb stands for "bar", implying reset with a bar over it. As such, the reset function is active low so a logic 0 is reset, while logic 1 is not reset. 2) To my knowledge, the only function...
  • RE: AD9508 Timing information about synchronization
    ADIApproved
    Hi Akira, Are you asking about any timing relationship between the input clock and the SYNCB signal? Are they interested in a setup and hold type number? The SYNCB can be asserted either through the...
 
Related Content
  • RE: Write EEPROM through ADAU1452
    DaveThib
    Hello Dovydas, It was as I thought might happen. When you trigger the soft reset it is just like toggling the reset pin and so the part selfboots. Since the PLL is already up and locked it seems to happen...
  • RE: Question about AD9910 "resetb" bit of CFR3..
    ADIApproved
    1) The "b" in resetb stands for "bar", implying reset with a bar over it. As such, the reset function is active low so a logic 0 is reset, while logic 1 is not reset. 2) To my knowledge, the only function...
  • RE: AD9508 Timing information about synchronization
    ADIApproved
    Hi Akira, Are you asking about any timing relationship between the input clock and the SYNCB signal? Are they interested in a setup and hold type number? The SYNCB can be asserted either through the...