Analog.com
Analog
Dialogue
Wiki
简体中文
EngineerZone
Search
Log in
Site
Search
Log in
Home
Blogs ⌵
EngineerZone Spotlight
The Engineering Mind
Analog Garage
Browse ⌵
All Groups
All Members
Support ⌵
3D ToF Depth Sensing
Amplifiers
Analog Microcontrollers
Audio
Clock and Timing
Data Converters
Design Tools and Calculators
Direct Digital Synthesis (DDS)
Embedded Vision Sensing
Energy Monitoring and Metering
FPGA Reference Designs
Industrial Ethernet
Interface and Isolation
Low Power RF Transceivers
MeasureWare
MEMS Inertial Sensors
Motor Control Hardware Platforms
Optical Sensing
Power By Linear
Processors and DSP
Reference Circuits
RF and Microwave
Switches/Multiplexers
Temperature Sensors
Video
Wireless Sensor Networks Reference Library
My EZ
More
Cancel
Clock and Timing
Documents
AD9552 loop bandwidth and PFD rate?
Q&A
Discussions
Documents
File Uploads
Video/Images
Tags
Reports
More
Cancel
New
Clock and Timing requires membership for participation - click to join
+
Documents
AD9508 in CMOS Single-Ended Output Configuration
AD9510 Register Configuration Reset
AD9510: datasheet appears to contradict evaluation board schematic which uses balun for single ended ref clock connection.
AD9510: Evaluation PCB
AD9510: Outputs not in Phase
AD9511: Programming the device in RESET
AD9512 evaluation board and Windows 7, 64 Bit driver issues
AD9512 evaluation software and windows 7 64bit compatibleissues
AD9512 Phase setting not working
AD9513: figure 25 full scale delay datasheet error
AD9515_power consumption with divider ratio
AD9517-1 delay to output of channel divider
AD951x: REFIN & CLK levels and FAQ "how to treat unused pins"
AD9520-3 EEPROM settings aren't loaded
AD9523-1: Can I bypass PLL1 and only use the PLL2?
AD9548 v AD9518, comparison of phase noise performance
AD9548: JTAG simulation file
AD9549BCPZ:P CMOS does not have output
AD9552 loop bandwidth and PFD rate?
ADCLK846: broadband jitter description
Additive and Absolute Jitter
Baking the AD9951A
Clock and Timing Support Community
FAQ: Does the AD9523, AD9524, or AD9523-1 have glitchless switchover?
HMC7044, HMC7043 vs LTC6952, LTC6953
Holdover/Switchover Functionality
Jitter over Multiple Bandwidths
LTC695x Low Frequency Phase Noise Measurement Issues
LVDS specifications
RE: AD9514 synchronisation setup and hold times of SYNCB with respect to CLK/CLKB
Want to use AD9510/11's DLD as our lock alarm, but it may not work properly if the reference disappears. Any solution?
What's the best way to connect a 3.3V CMOS clock signal to SYSCLK?
Why is the minimum Input Frequency for the Single-Ended Mode REF1 and REF2 AC-Coupled only 20MHz?
AD9552 loop bandwidth and PFD rate?
Q
Would you please tell me the bandwidth of the Loop Filter? And if the PD(Phase
detect) Frequency is 10kHz, AD9552's output is 300kHz or 3MHz, then how about
the spur performance of the output?
A
The AD9552 loop bandwidth is 50KHz. The charge pump current is linked to the N
feedback divider division value so when the N division is changed the charge
pump current is changed by the same percentage to maintain constant bandwidth.
The PFD rate is the reference input frequency or 2x if the doubler is turned
on. If the input frequency is below 16MHz (by selecting A2:A0) the doubler
will automatically turn on.
We don’t have a guaranteed spurious spec in the tables. With a fractional PLL
with a lot of flexibility it is difficult to do this. There could be more than
one configuration that can achieve the same output frequency, often I suggest
to try them to see which gives the desired spurious performance.
ad9552
Share
History
More
Cancel
Comments
Related