can EVAL-AD9516-0 keeps the register setup?

Hi,

I want to use EVAL-AD9516-0 as clock source for AD9208. 

I know that EVAL-AD9516-0 has convenient software.

I wonder if the settings are stored when I set up the settings using the software.

So, I wonder if EVAL-AD9516-0 keeps the settings even if I turn off the system and turn it back on without the software.