Dear Sir,
I have a question regarding use of AD9545/AD9546 as IEEE 1588 Servo which you may be able to clarify.
Let's suppose that I have board with SoC unit (running Linux) that controls AD9545 that is located on the board as well. The board receives IEEE 1588 SyncE synchronization signals that are processed by the SoC unit which extracts from it a reference signal of 156.25 MHz which feeds AD9545 (e.g. REFA). Then signal with the same frequency is synthesized also on one of the outputs (e.g. OUT0 A) and goes back to the SoC creating essentially a loop so I have frequency synchronization based on SyncE. The essential question is what more has to be implemented to get PTP synchronization? Given SoC is able to process the TSU (Time Stamp Unit) with the external Grandmaster, so can eventually also source 1 PPS signal for the AD9545.
I know that for example in the Renesas ClockMatrix IEEE Synchronizers device family the whole solution is based on above approach (but without 1 PPS signal, only 156.25 MHz signal going in the loop between external; ) using official linux kernel drivers from Renesas that are part of main Linux line as a part of the "ptp4l" apt which does all the work with the phase adjustements, etc. via SPI/I2C writings to the clock synchronizer. On the other hand I can see Analog Devices does not provide such offcial drivers to be used with "ptp4l" - how does PTP + SyncE can be implemented in such a system as synchronization unit? Do I think correctly that in order to implement such a system using AD9545 there should be two reference signals going to the AD9545: one 156.25 MHz SyncE (which provides frequency stability reference) and second - 1 PPS (which provides PTP phase synchronization information)? Then I would like to synthesize 156.25 MHz output (going to the SoC), 10 MHz (as output reference), 1 PPS (as output reference), 7.68 MHz and 122.88 MHz that would be used as reference by JESD204B jitter cleaner.
Is it possible to set one of the PLLs (that is PTP 1 PPS referenced) to control second PLL (that is SyncE 156.26 MHz referenced) in terms of their phases to have the SyncE's frequency stability for all the output signals and phase aligment from the PTP? Could you provide me with the example file with such settings to test?
Best regards