Post Go back to editing

AD-FMCDAQ2-EBZ reference design from the ZCU102 platform to an ALINX AXU15EG (ZU15EG)

Thread Summary

The user is porting the AD-FMCDAQ2-EBZ reference design to an ALINX AXU15EG (ZU15EG) board and encounters an AD9523 SPI write-verify failure, returning 0x00FF. The final answer suggests that 0xFF indicates the device is in reset or not powered on, and recommends checking the power and reset conditions of the AD9523. Relevant products: AD-FMCDAQ2-EBZ, AD9523, ZCU102, AXU15EG.
AI Generated Content
Category: Software
Product Number: AD-FMCDAQ2-EBZ
Software Version: ADI no-OS 2023_r2 Release

Hello ADI Team,

I am currently porting the AD-FMCDAQ2-EBZ reference design from the ZCU102 platform to an ALINX AXU15EG (ZU15EG) evaluation board. Since the AXU15EG is not officially supported, I used the ZCU102 design as a reference.

Hardware

  • Carrier board: ALINX AXU15EG (XCZU15EG)

  • FMC board: AD-FMCDAQ2-EBZ

  • Vivado: 2023.2

  • Vitis: 2021.2

  • Software: ADI no-OS (bare-metal) 2023_r2 Release

Step 1 – Vivado Hardware Porting

I first created a Vivado 2023.2 project by starting from the ZCU102 DAQ2 reference design.

The modifications included:

  • Replacing the ZCU102 board with the AXU15EG device.

  • Updating all board constraints (.xdc) according to the AXU15EG FMC HPC connector.

  • Verifying:

    • JESD204 transceiver lane mapping

    • Differential clock pins

    • SYSREF

    • SYNC signals

    • SPI signals

    • GPIO assignments

  • The design was implemented successfully and the bitstream was generated without critical errors.

Step 2 – Bare-Metal Software

I then created a Vitis bare-metal application using the ADI no-OS framework.

The software is based on the standard FMCDAQ2 example application without major modifications except for the platform-specific BSP.

The application starts correctly until the initialization of the AD9523 clock generator.

The console output reports:

AD9523: SPI write-verify failed (0x00FF)!

The failure occurs during ad9523_setup().


Debug Information

The SPI initialization completes successfully.

The failure happens when the driver performs a write followed by a read-back verification.

The read-back value is:

0x00FF

instead of the expected value.

From debugging, the failure occurs inside:

ad9523_setup()
ad9523_spi_write()
ad9523_spi_read()
SPI write-verify failed


What I Have Already Checked

  • SPI pin assignments match the AXU15EG schematic.

  • SPI clock, MOSI, MISO and CS are connected correctly.

  • FMC connector routing has been verified.

  • The FPGA bitstream programs correctly.

My Questions

  • Has anyone successfully ported the FMCDAQ2 reference design to a non-supported Zynq UltraScale+ board?
  • What could cause the AD9523 SPI read-back to always return 0x00FF?
  • Are there any recommended debug steps to isolate whether the problem is hardware, HDL, or software?
  • Any suggestions would be greatly appreciated.

Thank you.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.