Post Go back to editing

TX1 and TX2 recommanded matching network

Category: Hardware
Product Number: AD9375

Hi,

we are planing to use the AD9375 in the frequency band of 300 to 1000Mhz. From the UG-992 p.252 , we have to use the following components for the following circuit (See images below).

So, we have to use the B0322J5050AHF. From the component, it seems that L305 must be added, however, the conversation at this link tells that the L305 is DNI:


https://ez.analog.com/rf/wide-band-rf-transceivers/design-support-ad9371/f/q-a/575671/b0322j5050ahf-for-ad9371-s-tx-port

I am a little confuse by that answer, so i just want to validate if i have to put L305 between Pin 2 and Pin 3, but not to pin 4?

Thank you very much and have a nive day!