Post Go back to editing

ADCLK944 jitter

Thread Summary

The user asked about the jitter added by the ADCLK944 buffer when input signals are 10MHz and 100MHz. The final answer indicates that the ADCLK944 adds additive jitter, which can be found in the specification table of the data sheet.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADCLK944

What is the jitter of ADCLK944 when the input signals are 10MHz and 100Mhz?

Parents
  • Thank you for your reply. However, the data sheet only provides the additive jitter under the 1GHz condition, but does not give the additive jitter for 10MHz and 100MHz conditions. It can be seen from the data sheets of other's buffers that the lower the frequency, the larger the jitter is. As shown in the following figure:

Reply
  • Thank you for your reply. However, the data sheet only provides the additive jitter under the 1GHz condition, but does not give the additive jitter for 10MHz and 100MHz conditions. It can be seen from the data sheets of other's buffers that the lower the frequency, the larger the jitter is. As shown in the following figure:

Children