Hi Team,
I am experimenting recently with AD9510 evaluation board with a dedicated control software to upload the configuration. I am using AD9510 in a configuration where my REF is a 25 MHz signal coming from an OCXO (ECOC‑9775‑25), and my CLK2 comes from Crystek's VCXO operating at 100 MHz (CVHD-950-100). Here are the phase noise of these two parts (OCXO and VCXO, respectively):
and 
Using the AdiSimCLK I design the loop filter for the system to get a clean 100 MHz at the output. The discrepancy between the expectations and the measurements are quite large. While the noise should go well below -150 dBc/Hz already at offsets > 10k, in my case it hovers above -150 dBc/Hz all the way up (just like this):


My loop filter bandwidth is ca. 1 kHz. It seems that it works, The largest differences are outside the loop bandwidth. The apparent bump @300Hz must be some artefact as measurements with a different, and typically poorer instrument (a regular spectrum analyser with phase-noise option) show a better behaviour closer to what is simulated (ca. -120 dBc/Hz @1kHz). Anyways, I hoped for a bit better numbers (closer to -160 dBc/Hz @>100k, as predicted based on VCXO behaviour far off the carrier).
My questions:
1) Are the noise floor at ca. -150 dBc/Hz something to be expected from AD9510? Could be that the increased phase noise observed in my experiments comes results from the fact that my EVAL does not have any filtering section on the DVDD/AVDD at the edge of the PCB?
2) Are there any measurements available (done with the EVAL) showing typical performance of the board (something like the phase noise curves available in catalogue notes for parts like AD9545)?
It case it matters, please find attached the session file
"AD9510 Setup File" "Rev","1.0" "" "Addr(Hex)","Value(Bin)","Value(Hex)" "00","00010000","10" "02","00100000","20" "04","00000000","00" "05","00000000","00" "06","00000100","04" "07","01100000","60" "08","01010111","57" "09","00000000","00" "0A","00000010","02" "0B","00000000","00" "0C","00000000","00" "0D","00000000","00" "34","00000001","01" "35","00000000","00" "36","00000000","00" "37","00000100","04" "38","00000001","01" "39","00000000","00" "3A","00000000","00" "3B","00000100","04" "3C","00001010","0A" "3D","00001011","0B" "3E","00001011","0B" "3F","00001011","0B" "40","00000100","04" "41","00000011","03" "42","00000011","03" "43","00000011","03" "44","00010011","13" "45","00000010","02" "48","00000000","00" "49","00000000","00" "4A","00000000","00" "4B","00000000","00" "4C","00010001","11" "4D","00000000","00" "4E","00110011","33" "4F","00000000","00" "50","00000000","00" "51","10000000","80" "52","00010001","11" "53","00000000","00" "54","00000000","00" "55","00000000","00" "56","00000000","00" "57","00000000","00" "58","00100000","20" "59","00000000","00" "5A","00000000","00" "" "Other Settings..." "RefIn:",25 "CLKInp1:",1200 "CLKInp2:",100 "CPRSet:",5100 "Auto Update:",1 "Load All Regs:",1
Regards
Pawel