Post Go back to editing

timer never times out if Trigger stays high.

Thread Summary

The user asked if keeping the trigger pin high on a device causes the output to stay high, indicating level sensitivity. The support engineer clarified that the LTC6993-2 requires a low-to-high transition on the TRIG pin to generate a pulse, and keeping the pin high does not sustain the output. The TRIG pin's behavior is detailed in the data sheet, emphasizing the importance of proper triggering.
AI Generated Content
Category: Hardware
Product Number: LTC6993HDCB-2, LTC699

if the the trigger pin is kept high, the output never times out, i.e. stays high

is this device level sensitive?

any application notes that can help will be appreciated

Thank you

Fausto bartra

circuit below

  • Hi,

    sorry for getting back to you so late.

    You need to toggle TRIG low to high in order for the LTC6993-2 to generate a pulse.

    Did you toggle TRIG?

    This is the spec of TRIG from page 5 of the data sheet:

    Petre

  • Petre:

    Thank you for your reply

    Yes I understand that I need to toggle this pin for it to work

    The device is configured to POL = 0, so the one shot output pulses are high

    Only one board is behaving this way.

    This is happening at power up.

    The situation is at power up the TRIG pin stays high and the output pin also stays high

    My understanding is that the output pin should go low after it times out.

    But it never goes down.

    if the TRIG pin stays high then the output will stay high <== this is my question

    Thank you

    Fausto

  • HI,

    "if the TRIG pin stays high then the output will stay high <== this is my question"

    No. In the data sheet, at page 14 it is stated that a rising edge on TRIG initiates the output pulse and the output pulse is determined by NDIV and RSET, not by the fact the TRIG signal stays high or low. So even if the TRIG stays high, the pulse should go low after approximately 30s (if I calculated well based on your schematic)

    There is also a possibility of multiple TRIG pulses that can keep the output high indefinitely. See how the TRIG behaves.

    Usually, in such cases in which only one board does not function as expected and the others do, I recommend replacing the LTC6933 with a chip from a board that is functional. If the problem is solved, the previous chip was bad and if you want, you may contact your ADI representative to initiate a failure analysis. If the problem is not solved, you have a problem on the board and you'll have to debug it.

    Petre