Hello there!
I am working on AD9523-1 board and from that i want to generate 122.8800 fixed output clock but the poblem is that i configured the o/p of PLL2 is exactly 122.88 i see on frequency counter it is started from 122.8745123 and increasing gradually in Hz and after 2 hours it is increasing from 122.880000 to onwards i mean to say lets suppose after 2 hours it is 122.889909. i need stable clock output which is 122.880000. I have given you the .stp file that i follow as well as i have given you all the configuration screenshoots following that i have changed. Secondly i want to give external refernce frequency by signal generater but it is taking internally guide me how i can give the extertnal frequency.
please resolve the problem i want exact stable 122.88 MHz output and if possile give me .stp configuration file i am very thankful to you.
Thanks
;Header contains information about the setup file and revision
<Header>
Product = AD9523-1
FileVersion = 1.0
DecimalSeparator=. ;Used for internationalization
</Header>
<RegisterMap>
&h0,&b00000001 ;01 Hex, 001 Dec
&h2,&b00000000 ;00 Hex, 000 Dec
&h3,&b00000000 ;00 Hex, 000 Dec
&h4,&b00000000 ;00 Hex, 000 Dec
&h5,&b00000000 ;00 Hex, 000 Dec
&h6,&b00000000 ;00 Hex, 000 Dec
&h10,&b00000001 ;01 Hex, 001 Dec
&h11,&b00000000 ;00 Hex, 000 Dec
&h12,&b00000100 ;04 Hex, 004 Dec
&h13,&b00000000 ;00 Hex, 000 Dec
&h14,&b00000001 ;01 Hex, 001 Dec
&h15,&b00000000 ;00 Hex, 000 Dec
&h16,&b00101000 ;28 Hex, 040 Dec
&h17,&b00000000 ;00 Hex, 000 Dec
&h18,&b00001100 ;0C Hex, 012 Dec
&h19,&b00011111 ;1F Hex, 031 Dec
&h1A,&b00010010 ;12 Hex, 018 Dec
&h1B,&b00010110 ;16 Hex, 022 Dec
&h1C,&b10010000 ;90 Hex, 144 Dec
&h1D,&b00000000 ;00 Hex, 000 Dec
&h1E,&b00000000 ;00 Hex, 000 Dec
&h1F,&b00000000 ;00 Hex, 000 Dec
&h20,&b00000000 ;00 Hex, 000 Dec
&hF0,&b00000111 ;07 Hex, 007 Dec
&hF1,&b10000111 ;87 Hex, 135 Dec
&hF2,&b00010011 ;13 Hex, 019 Dec
&hF3,&b00000010 ;02 Hex, 002 Dec
&hF4,&b01000000 ;40 Hex, 064 Dec
&hF5,&b00000000 ;00 Hex, 000 Dec
&hF6,&b00000000 ;00 Hex, 000 Dec
&hF7,&b00000001 ;01 Hex, 001 Dec
&hF8,&b00000000 ;00 Hex, 000 Dec
&hF9,&b00000000 ;00 Hex, 000 Dec
&hFA,&b00000000 ;00 Hex, 000 Dec
&h190,&b01110011 ;73 Hex, 115 Dec
&h191,&b00001001 ;09 Hex, 009 Dec
&h192,&b00000100 ;04 Hex, 004 Dec
&h193,&b00100000 ;20 Hex, 032 Dec
&h194,&b00011111 ;1F Hex, 031 Dec
&h195,&b00000100 ;04 Hex, 004 Dec
&h196,&b01001000 ;48 Hex, 072 Dec
&h197,&b00001001 ;09 Hex, 009 Dec
&h198,&b00000000 ;00 Hex, 000 Dec
&h199,&b01110110 ;76 Hex, 118 Dec
&h19A,&b00011111 ;1F Hex, 031 Dec
&h19B,&b00000100 ;04 Hex, 004 Dec
&h19C,&b01001000 ;48 Hex, 072 Dec
&h19D,&b00001001 ;09 Hex, 009 Dec
&h19E,&b00000000 ;00 Hex, 000 Dec
&h19F,&b00100000 ;20 Hex, 032 Dec
&h1A0,&b00011111 ;1F Hex, 031 Dec
&h1A1,&b00000100 ;04 Hex, 004 Dec
&h1A2,&b00100000 ;20 Hex, 032 Dec
&h1A3,&b00011111 ;1F Hex, 031 Dec
&h1A4,&b00000100 ;04 Hex, 004 Dec
&h1A5,&b00100000 ;20 Hex, 032 Dec
&h1A6,&b00011111 ;1F Hex, 031 Dec
&h1A7,&b00000100 ;04 Hex, 004 Dec
&h1A8,&b01100110 ;66 Hex, 102 Dec
&h1A9,&b00001001 ;09 Hex, 009 Dec
&h1AA,&b00000100 ;04 Hex, 004 Dec
&h1AB,&b01001001 ;49 Hex, 073 Dec
&h1AC,&b00001001 ;09 Hex, 009 Dec
&h1AD,&b00000000 ;00 Hex, 000 Dec
&h1AE,&b01001001 ;49 Hex, 073 Dec
&h1AF,&b00001001 ;09 Hex, 009 Dec
&h1B0,&b00000000 ;00 Hex, 000 Dec
&h1B1,&b01101000 ;68 Hex, 104 Dec
&h1B2,&b00001001 ;09 Hex, 009 Dec
&h1B3,&b00000100 ;04 Hex, 004 Dec
&h1B4,&b01101000 ;68 Hex, 104 Dec
&h1B5,&b00001001 ;09 Hex, 009 Dec
&h1B6,&b00000100 ;04 Hex, 004 Dec
&h1B7,&b01010110 ;56 Hex, 086 Dec
&h1B8,&b00001001 ;09 Hex, 009 Dec
&h1B9,&b00000000 ;00 Hex, 000 Dec
&h1BA,&b00000000 ;00 Hex, 000 Dec
&h1BB,&b00000000 ;00 Hex, 000 Dec
&h22C,&b00000000 ;00 Hex, 000 Dec
&h22D,&b00000000 ;00 Hex, 000 Dec
&h22E,&b00000000 ;00 Hex, 000 Dec
&h22F,&b00000000 ;00 Hex, 000 Dec
&h230,&b00000000 ;00 Hex, 000 Dec
&h231,&b00000001 ;01 Hex, 001 Dec
&h232,&b00000000 ;00 Hex, 000 Dec
&h233,&b00000000 ;00 Hex, 000 Dec
&h234,&b00000001 ;01 Hex, 001 Dec
&hA00,&b00000000 ;00 Hex, 000 Dec
&hA01,&b00000000 ;00 Hex, 000 Dec
&hA02,&b00000000 ;00 Hex, 000 Dec
&hA03,&b00000010 ;02 Hex, 002 Dec
&hA04,&b00000000 ;00 Hex, 000 Dec
&hA05,&b00000100 ;04 Hex, 004 Dec
&hA06,&b00001110 ;0E Hex, 014 Dec
&hA07,&b00000000 ;00 Hex, 000 Dec
&hA08,&b00010000 ;10 Hex, 016 Dec
&hA09,&b00001110 ;0E Hex, 014 Dec
&hA0A,&b00000000 ;00 Hex, 000 Dec
&hA0B,&b11110000 ;F0 Hex, 240 Dec
&hA0C,&b00101011 ;2B Hex, 043 Dec
&hA0D,&b00000001 ;01 Hex, 001 Dec
&hA0E,&b10010000 ;90 Hex, 144 Dec
&hA0F,&b00000001 ;01 Hex, 001 Dec
&hA10,&b00000001 ;01 Hex, 001 Dec
&hA11,&b11100000 ;E0 Hex, 224 Dec
&hA12,&b00000011 ;03 Hex, 003 Dec
&hA13,&b00000010 ;02 Hex, 002 Dec
&hA14,&b00110000 ;30 Hex, 048 Dec
&hA15,&b10000000 ;80 Hex, 128 Dec
&hA16,&b11111111 ;FF Hex, 255 Dec
&hB00,&b00000000 ;00 Hex, 000 Dec
&hB01,&b00000000 ;00 Hex, 000 Dec
&hB02,&b00000000 ;00 Hex, 000 Dec
&hB03,&b00000000 ;00 Hex, 000 Dec
</RegisterMap>
<PinStates>
PortA=&h1E ;Bit0=USBStatus, Bit1=CSB, Bit2=ResetB, Bit3=SyncB, Bit4=PDB, Bit5=RefSel
</PinStates>
<SoftwareSettings>
AutoSendUpdate=1 ;AutoIOUpdate Setting
REF_A = 10.0000
REF_B = 10.0000
REF_TEST = 10.0000
VCXO = 100.0000
</SoftwareSettings>