Hi, what is the maximum current consumption of AD9511? The datasheet does not contain this information.
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 0 hours |
pminc48 |
Closed |
AD9511
Recommended for New Designs
The AD9511 provides a multi-output clock distribution function along with an on-chip PLL core. The design emphasizes low jitter and phase noise to maximize...
Datasheet
AD9511 on Analog.com
Hi, what is the maximum current consumption of AD9511? The datasheet does not contain this information.
HI,
the data sheet provides the power dissipation of 800mW or 850 mW max:

If the VS=3.3V+/-5% and we use VCP=VS, then the max current consumption may be determined: 0.850/3.3=0.257A.
Note this does not include the power dissipated in the external resistors.
Petre