Post Go back to editing

10 MHz input frequency to 122.8 MHz differential output

Thread Summary

The user seeks to input a 10MHz single-ended signal and output a 122.8MHz differential signal using the AD9576 evaluation board. The final answer recommends setting jumpers SP1 and SP0 towards HIGH for SPI communication, and applying the 10MHz signal to REF0P with jumpers P207 and P208 set to DIFF. The provided configuration file (AD9576_setup.cso.txt) should be used to achieve the desired output, with all outputs set to LVDS.
AI Generated Content
Category: Hardware
Product Number: AD9576

Hello,

I am Chris a student engineer. I am engaged in a project which has to do with clock distribution. 

I recently purchased the AD9576 evaluation board and I want to input a 10MHz signal and output it at 122.8MHz. I installed ACE software and the plugins that were needed. I have read the documentation of the product and some days now I am getting familiar with the board and the software, but I am facing some issues. Below I will enumerate and write down my concerns.

1) I am confused with the jumpers settings and the options of the register programming through the Memory Map. Do I need to place the jumpers in specific states to be able to program through the software, or should i remove all the jumpers and after everything is programmable?

2) My goal is to input a 10MHz signal (single ended) and output it to 122.8 MHz(differential signal), is someone capable to provide me with the path i need to follow to output this 122.8 MHz signal, and also provide me with the settings i need to configure on the board (possible pin strapping on the pins of REF0, REF1 an REF2 and PPR settings, if needed).

Thank you Slight smile,

Chris 

Thread Notes

  • HI,

    " I am confused with the jumpers settings and the options of the register programming through the Memory Map. Do I need to place the jumpers in specific states to be able to program through the software, or should i remove all the jumpers and after everything is programmable?"

    If you want to use the PPRx pins to configure the AD9576, you need to leave the pins SP1 and SP0 floating at jumpers P102 and P103. 

    For the rest of the jumpers, see a photo of the board I use. I set SP1 and SP0 towards label HIGH, so the AD9576 only uses SPI communication to be configured.

    "My goal is to input a 10MHz signal (single ended) and output it to 122.8 MHz(differential signal), is someone capable to provide me with the path i need to follow to output this 122.8 MHz signal, and also provide me with the settings i need to configure on the board (possible pin strapping on the pins of REF0, REF1 an REF2 and PPR settings, if needed)."

    PDF

    Let's say you apply 10MHz clock from a signal generator. I usually use 3dBm as amplitude. Let's say we want to apply it at REF0P, J201. Put the jumpers P207 and P208 towards DIFF label.

    This is the configuration I propose:

    AD9576_setup.cso.txt

    Take the txt extension from the attached cso file before loading it into ACE. I did not test it on an eval board, but it should work.

    The outputs are all LVDS and this matches the schematic.

    Petre

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.